How to configure iMX6UL CLK1_P/N as output pin

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to configure iMX6UL CLK1_P/N as output pin

跳至解决方案
1,154 次查看
freescale_jive
Contributor II

Hello, I would like to check:

1. Are the signals CCM_CLK1_P/N described in iMX6UL datasheet correspond to the pin CLK1_P/N ?

2. The datasheet mentioned that these 2 signals can be used "To output internal SoC clock to be used outside....".

May I know which section in iMX6UL RM describes how to do it? what are the registers? how to select clock source and divider etc ?

3. The closest description I can find in RM is "CCM_CLKO1/2". Are these signals routed to CLK1_P/N pins ?

Thanks!

Thomas

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
876 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Thomas

configuration is described in sect.38.6.6 Miscellaneous Register 1 (PMU_MISC1n)

field LVDS1_CLK_SEL, i.MX6UL Reference Manual (rev.0  8/2015)

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6ULRM.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
877 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Thomas

configuration is described in sect.38.6.6 Miscellaneous Register 1 (PMU_MISC1n)

field LVDS1_CLK_SEL, i.MX6UL Reference Manual (rev.0  8/2015)

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6ULRM.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复