Hi All,
I am using my custom board which is similar to sabresd board in want to configure the below given gpio's in dts file if any one knows can you please help me.
NOTE: kernel version is 3.14
(1,12) -- pwn-gpio (output high)
(1,13) -- rst-gpio (output high)
(1,7) -- camera enable (it should be "output high" )
I given like this
ov1062x: ov1062x@30 {
compatible = "ovti,ov1062x";
reg = <0x30>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_ipu1_2>;
clocks = <&clks IMX6QDL_CLK_CKO>;
clock-names = "csi_mclk";
DOVDD-supply = <&vgen4_reg>; /* 1.8v */
AVDD-supply = <&vgen3_reg>; /* 2.8v, on rev C board is VGEN3,
/* on rev B board is VGEN5 */
DVDD-supply = <&vgen2_reg>; /* 1.5v*/
pwn-gpios = <&gpio1 12 1>;
rst-gpios = <&gpio1 13 1>;
enable-gpios = <&gpio1 7 1>;
csi_id = <0>;
mclk = <24000000>;
mclk_source = <0>;
};
In other place where and all i need to give to work my camera properly.
And one more issue i am facing, whenever i am inserting mxc_v4l2_capture.ko it is giving
ERROR:V4l2 Slave not found!
But i inserted my driver before inserting mxc_v4l2_capture.ko
Can any one please hep me to sort it out , Thanks in advance.
Thanks & Regards,
Lavanya
已解决! 转到解答。
Hi igorpadykov ,
Thank you i2c SDA line problem is there the camera board to Main board DVP cable is not working properly so we replaced that,
Now i can able to capture the video.
Thanks & Regards,
Lavanya
Hi igorpadykov ,
Thank you i2c SDA line problem is there the camera board to Main board DVP cable is not working properly so we replaced that,
Now i can able to capture the video.
Thanks & Regards,
Lavanya
Hi Bandaru
one can look at example in imx6qdl-sabresd.dtsi :
pwn-gpios = <&gpio1 16 1>; /* active low: SD1_DAT0 */
rst-gpios = <&gpio1 17 0>; /* active high: SD1_DAT1 */
check how these pins are parsed and add any other control gpio, if necessary using sources
linux/drivers/media/platform/mxc/capture/ov5640.c
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igorpadykov,
If i give like this dts file can i see these pins in /sys/kernel/debug/gpio
pwn-gpios = <&gpio1 16 1>; /* active low: SD1_DAT0 */
rst-gpios = <&gpio1 17 0>; /* active high: SD1_DAT1 */
Thanks & Regards,
Lavanya
Hi igorpadykov,
Now my PWDN and RST pins are configured properly.
But i am not getting any clock in CSI_MCLK or PCLK.
When i probed i can able to get MCLK and RST and PWDN are proper but in dmesg it is giving like below
12 pwn_pin
13 reset_pin
-2046695040 csi_mclk
24000000 mclk
0 mclk_source
0 csi_id
ov5640_read_reg:write reg error:reg=300a
camera ov5640 is not found
My dts Configurations are below
ov564x: ov564x@3c {
compatible = "ovti,ov564x";
reg = <0x3c>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_ipu1_2>;
clocks = <&clks IMX6QDL_CLK_CKO>;
clock-names = "csi_mclk";
DOVDD-supply = <&vgen4_reg>; /* 1.8v */
AVDD-supply = <&vgen3_reg>; /* 2.8v, on rev C board is VGEN3,
on rev B board is VGEN5 */
DVDD-supply = <&vgen2_reg>; /* 1.5v*/
/*pwn-gpios = <&gpio1 16 1>; active low: SD1_DAT0
rst-gpios = <&gpio1 17 0>; active high: SD1_DAT1 */ //using for wifi in FS_WCAM
pwn-gpios = <&gpio1 12 GPIO_ACTIVE_HIGH>; /* FS_WCAM active high: SD2_DAT3 */
rst-gpios = <&gpio1 13 GPIO_ACTIVE_LOW>; /* FS_WCAM active low: SD2_DAT2 */
csi_id = <0>;
mclk = <24000000>;
mclk_source = <0>;
};
pinctrl_ipu1_2: ipu1grp-2 { /* parallel camera */
fsl,pins = <
MX6QDL_PAD_CSI0_DAT12__IPU1_CSI0_DATA12 0x80000000
MX6QDL_PAD_CSI0_DAT13__IPU1_CSI0_DATA13 0x80000000
MX6QDL_PAD_CSI0_DAT14__IPU1_CSI0_DATA14 0x80000000
MX6QDL_PAD_CSI0_DAT15__IPU1_CSI0_DATA15 0x80000000
MX6QDL_PAD_CSI0_DAT16__IPU1_CSI0_DATA16 0x80000000
MX6QDL_PAD_CSI0_DAT17__IPU1_CSI0_DATA17 0x80000000
MX6QDL_PAD_CSI0_DAT18__IPU1_CSI0_DATA18 0x80000000
MX6QDL_PAD_CSI0_DAT19__IPU1_CSI0_DATA19 0x80000000
// MX6QDL_PAD_CSI0_DATA_EN__IPU1_CSI0_DATA_EN 0x80000000
MX6QDL_PAD_CSI0_PIXCLK__IPU1_CSI0_PIXCLK 0x80000000
MX6QDL_PAD_CSI0_MCLK__IPU1_CSI0_HSYNC 0x80000000
MX6QDL_PAD_CSI0_VSYNC__IPU1_CSI0_VSYNC 0x80000000
MX6QDL_PAD_SD2_DAT2__GPIO1_IO13 0x80000000
MX6QDL_PAD_SD2_DAT3__GPIO1_IO12 0x80000000
>;
};
Kindly Help me how can i solve this issue.