Out project is based on iMX6 Dual core and Ubuntu, I have tested that the totem media player is very powerful and very suit for us except that we may do some customization for UI.
But after I did ./configure in the totem-3.0.1 source code directory, it complained that several packages were need for the build. I tried to search gtk+3.0 with "apt-cache search" command, but there is no result.
I want to ask how to configure and build totem 3.0.1, and if Freescale did some modifications on the source code of totem-3.0.1.
Below is the configuration log. And I also upload the totem 3.0.1 source code in the attachment.
=====================================================================================
checking whether to enable maintainer-specific portions of Makefiles... no
checking for a BSD-compatible install... /usr/bin/install -c
checking whether build environment is sane... yes
checking for a thread-safe mkdir -p... /bin/mkdir -p
checking for gawk... no
checking for mawk... mawk
checking whether make sets $(MAKE)... yes
checking whether NLS is requested... yes
checking for style of include used by make... GNU
checking for gcc... gcc
checking whether the C compiler works... yes
checking for C compiler default output file name... a.out
checking for suffix of executables...
checking whether we are cross compiling... no
checking for suffix of object files... o
checking whether we are using the GNU C compiler... yes
checking whether gcc accepts -g... yes
checking for gcc option to accept ISO C89... none needed
checking dependency style of gcc... gcc3
checking for intltool >= 0.40.0... 0.50.2 found
checking for intltool-update... /usr/bin/intltool-update
checking for intltool-merge... /usr/bin/intltool-merge
checking for intltool-extract... /usr/bin/intltool-extract
checking for xgettext... /usr/bin/xgettext
checking for msgmerge... /usr/bin/msgmerge
checking for msgfmt... /usr/bin/msgfmt
checking for gmsgfmt... /usr/bin/msgfmt
checking for perl... /usr/bin/perl
checking for perl >= 5.8.1... 5.14.2
checking for XML::Parser... ok
checking whether ln -s works... yes
checking for pkg-config... /usr/bin/pkg-config
checking pkg-config is at least version 0.9.0... yes
checking gnome-doc-utils >= 0.20.3... yes
checking for gobject-introspection... no
checking for g++... g++
checking whether we are using the GNU C++ compiler... yes
checking whether g++ accepts -g... yes
checking dependency style of g++... gcc3
checking whether gcc and cc understand -c and -o together... yes
checking build system type... armv7l-unknown-linux-gnueabi
checking host system type... armv7l-unknown-linux-gnueabi
checking how to print strings... printf
checking for a sed that does not truncate output... /bin/sed
checking for grep that handles long lines and -e... /bin/grep
checking for egrep... /bin/grep -E
checking for fgrep... /bin/grep -F
checking for ld used by gcc... /usr/bin/ld
checking if the linker (/usr/bin/ld) is GNU ld... yes
checking for BSD- or MS-compatible name lister (nm)... /usr/bin/nm -B
checking the name lister (/usr/bin/nm -B) interface... BSD nm
checking the maximum length of command line arguments... 1572864
checking whether the shell understands some XSI constructs... yes
checking whether the shell understands "+="... yes
checking how to convert armv7l-unknown-linux-gnueabi file names to armv7l-unknown-linux-gnueabi format... func_convert_file_noop
checking how to convert armv7l-unknown-linux-gnueabi file names to toolchain format... func_convert_file_noop
checking for /usr/bin/ld option to reload object files... -r
checking for objdump... objdump
checking how to recognize dependent libraries... pass_all
checking for dlltool... no
checking how to associate runtime and link libraries... printf %s\n
checking for ar... ar
checking for archiver @FILE support... @
checking for strip... strip
checking for ranlib... ranlib
checking command to parse /usr/bin/nm -B output from gcc object... ok
checking for sysroot... no
checking for mt... mt
checking if mt is a manifest tool... no
checking how to run the C preprocessor... gcc -E
checking for ANSI C header files... yes
checking for sys/types.h... yes
checking for sys/stat.h... yes
checking for stdlib.h... yes
checking for string.h... yes
checking for memory.h... yes
checking for strings.h... yes
checking for inttypes.h... yes
checking for stdint.h... yes
checking for unistd.h... yes
checking for dlfcn.h... yes
checking for objdir... .libs
checking if gcc supports -fno-rtti -fno-exceptions... no
checking for gcc option to produce PIC... -fPIC -DPIC
checking if gcc PIC flag -fPIC -DPIC works... yes
checking if gcc static flag -static works... yes
checking if gcc supports -c -o file.o... yes
checking if gcc supports -c -o file.o... (cached) yes
checking whether the gcc linker (/usr/bin/ld) supports shared libraries... yes
checking whether -lc should be explicitly linked in... no
checking dynamic linker characteristics... GNU/Linux ld.so
checking how to hardcode library paths into programs... immediate
checking whether stripping libraries is possible... yes
checking if libtool supports shared libraries... yes
checking whether to build shared libraries... yes
checking whether to build static libraries... yes
checking how to run the C++ preprocessor... g++ -E
checking for ld used by g++... /usr/bin/ld
checking if the linker (/usr/bin/ld) is GNU ld... yes
checking whether the g++ linker (/usr/bin/ld) supports shared libraries... yes
checking for g++ option to produce PIC... -fPIC -DPIC
checking if g++ PIC flag -fPIC -DPIC works... yes
checking if g++ static flag -static works... yes
checking if g++ supports -c -o file.o... yes
checking if g++ supports -c -o file.o... (cached) yes
checking whether the g++ linker (/usr/bin/ld) supports shared libraries... yes
checking dynamic linker characteristics... (cached) GNU/Linux ld.so
checking how to hardcode library paths into programs... immediate
configure: creating ./config.lt
config.lt: creating libtool
checking for pkg-config... (cached) /usr/bin/pkg-config
checking pkg-config is at least version 0.9.0... yes
checking for glib-genmarshal... /usr/bin/glib-genmarshal
checking for glib-mkenums... /usr/bin/glib-mkenums
checking whether to enable easy codec installation support... auto
checking for MISSING_PLUGINS... yes
checking for GST... yes
checking GStreamer 0.10 inspection tool... yes
checking GStreamer 0.10 playbin2 plugin... yes
checking GStreamer 0.10 ffmpegcolorspace plugin... yes
checking GStreamer 0.10 videoscale plugin... yes
checking GStreamer 0.10 gconfaudiosink plugin... yes
checking GStreamer 0.10 gconfvideosink plugin... yes
checking GStreamer 0.10 goom plugin... yes
checking which smclient backend to use... no
checking for DEPENDENCY... no
configure: error: Package requirements (
glib-2.0 >= 2.27.92
gio-2.0 >= 2.27.92
gtk+-3.0 >= 2.99.3
gdk-x11-3.0 >= 2.99.3
gmodule-2.0
totem-plparser >= 2.32.4
gstreamer-tag-0.10 >= 0.10.26
cairo) were not met:
No package 'gtk+-3.0' found
No package 'gdk-x11-3.0' found
No package 'totem-plparser' found
Consider adjusting the PKG_CONFIG_PATH environment variable if you
installed software in a non-standard prefix.
Alternatively, you may set the environment variables DEPENDENCY_CFLAGS
and DEPENDENCY_LIBS to avoid the need to call pkg-config.
See the pkg-config man page for more details.
Original Attachment has been moved to: totem_3.0.1.orig.tar.gz
Hi Frank,
The totem is opensource code, not in our support range, you could find solution for your issue in the internet
best regards
Jack