Hello Community,
I am working on iMX6 solo based custom board.I am setting some PAD control values in my U-boot code but that values are not reflecting after U-boot boots up. So, I want to change the PAD control values after U-boot boot up , say suppose I want to set 0x1b0b0 to UART control PADS. How can I do that using u-boot coomand?
I know I have to use the mw command , but when I tried mw 20e0330 1b0b0 and then I tried reading at that address using md 20e0330 it didn't change the values to 1b0b0.
Kindly help me to solve this issue.
Best Regards,
Hrushi
Hi Hrushi
could you try with mw.l and use nxp uboot 2016.03 :
http://git.freescale.com/git/cgit.cgi/imx/uboot-imx.git/tree/?h=imx_v2016.03_4.1.15_2.0.0_ga
Also as IOMUX Control (IOMUXC) registers are valid DCD address, one can set its value
in dcd header.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------