Hi community,
I have a quesion about i.MX6SDL OCOTP.
Please see chapter 47.3.1.3 in IMX6SDLRM Rev.2, it says as following.
"It should be noted that write latencies to OTP are numbers of 10 micro-seconds per word.
Write latencies is based on amount of bit filed which is 1. For example : program half
fuse bits in one word need 10 us x 16."
Then, how can I change the write latencies?
By HW_OCOTP_TIMING[STROBE_PROG]?
Best Regards,
Satoshi Shimoda
Hello,
Please follow recommendations of section 47.3.3 (OTP Read/Write Timing Parameters)
of the Reference Manual. Strictly speaking, it is not good idea to change significantly timings.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------