How to change i.MX 8M Quad Evaluation Kit, Win10 iot display resolution?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to change i.MX 8M Quad Evaluation Kit, Win10 iot display resolution?

930 次查看
alzip79
Contributor II

Hello. NXP

 

My Board : i.MX 8M Quad Evaluation Kit

My OS : windows 10 iot

 Using MCIMX8M-EVK Image FFU File,

When connected to a monitor that supports 3840x2160 resolution using the native HDMI port, it displays at 1280x720 resolution.

  

How to change to 3840x2160 Display Resolution?

 

Thank you for your help.

0 项奖励
回复
1 回复

803 次查看
jiri_rezler
NXP Employee
NXP Employee

Hello Sunjib

Windows 10 IOT display driver for 64bit (imx8MQ included) doesn't support change display resolution yet. HDMI initialization (display) is performed in u-boot code (see imx8mq_evk.c file), display resolution is configured to the fix value 1280x720 60Hz. You can modify  imx8mq_evk.c file in u-boot and HdLcdiMX8.c file in UEFI (mu_platform_nxp) on you own and rebuild u-boot & UEFI.

We plan to support of display resolution change in Windows 10 IOT display driver in future.

Best Regards

Jiri Rezler

0 项奖励
回复