How to add/edit LCD driver to support for 240x320 LCD

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to add/edit LCD driver to support for 240x320 LCD

680 次查看
danix
Contributor III

Hi all,

I have a custom board with Newhaven's 320x240 TFT LCD. it's a 24bpp dotclk LCd module with 4-wire resistive touch screen - which, by the way,

works with the default driver (lms430.c), exept outof range displays since lms430 is a 480x272 LCD.

I modified the timing, porches, etc.. in lms430.c, but the frame buffer driver doesn't seems to work correctly...

so what are all the modifications that I should make to support my panel properly?

Thanks

标记 (1)
0 项奖励
回复
0 回复数