Hello everyone, the board I use is MCIMX7SABRE. I only soldered the nor flash chip MX25L51245G on my board. So I want to burn the image into the nor flash. I am using MFG Tools L4.1.15_2.1.0. I used three methods: First, I started MfgTool2.exe directly, the program prompts in the partition, but the program seems to be stuck here. Second, I modified [LIST] name = Quad Nor Flash in cfg.ini. In this way, the program MfgTool2.exe can not be started, prompting an error. Third, I directly start mfgtool2-yocto-mx-sabresd-qspi-nor-mx25l51245g.vbs. In this way, the program will fail when the partition is erased.
My BOOT MODE is set to: Serial Downloader
I hope everyone can help me.
Hello, I see the information on the schematic that you mentioned above. So we changed a way to burn the image to emmc. We used another board with emmc, which is also the official website MCIMX7SABRE. When burning, MFG Tools is stuck in the partition interface. Can you guide me?