I am trying to use the feature of the i.MX6 processor to perform generic protection of data for secure storage in non-volatile memory. This is done by having the i.MX6 convert the data into a red blob (for general data). I found what I believe is a similar question from user fsquestion at https://community.freescale.com/message/340700. This question is marked as "Assumed Answered", but it was not. The only response is from Freescale, but is a response about Encrypted Boot (a completely separate topic). fsquestion has posted that they have still not figured out a way to do this, as current examples are limited to using the secure memory operations. This question does not deal with encrypted boot, just the handling en/de-capsulation of red blobs.
===========
I am attempting to wire a Linux driver to present a character interface that provides an IOCTL to allow user space applications to have a synchronous method to provide data to be en/de-capsulated into/out of red blobs and get the result. I am getting an error from the CAAM job, which tells me that something is wrong with the job descriptor:
1073743888
0x04 0x00 0x00 0x00 0x0008 0x0010
DESC IDX ERR: Inv. Seq Command
I tried to build up the descriptor using the following function, which is based on blob_encap_desc in sm_store.c, but modified to attempt to make red blobs to/from regular memory (not secure memory). I have not been able to figure out how to modify (or build) a proper CAAM job descriptor to perform the red blob en/de-capsulation.
/*
* Construct a in-memory red blob en/de-capsulation job descriptor
*
* - desc pointer to hold new (to be allocated) pointer to the generated
* descriptor for later use. Calling thread can kfree the
* descriptor after execution.
* - keymod Physical pointer to key modifier (contiguous piece).
* - keymodsz Size of key modifier in bytes (should normally be 8).
* - inbuf Physical pointer of the data to be en/de-capsulated.
* - outbuf Physical pointer (within an accessible secure memory page)
* of the encapsulated output. This needs to be larger than the
* input buffer by 48 bytes when performing encapsulation of the data.
* - inbuflen Size of input buffer, in bytes.
* - auth If nonzero, use AES-CCM for encapsulation, else use ECB
*
* Note: this uses 32-bit pointers at present
* retval: number of bytes in outbuf
*/
#define INITIAL_DESCSZ 16 /* size of tmp buffer for descriptor const. */
static int caam_blob_capsulate_desc(u32 **desc, dma_addr_t keymod, u16 keymodsz,
bool encap, dma_addr_t inbuf, dma_addr_t outbuf, u16 inbuflen,
bool auth)
{
u32 *tdesc, tmpdesc[INITIAL_DESCSZ];
u16 dsize, idx;
memset(tmpdesc, 0, INITIAL_DESCSZ * sizeof(u32));
idx = 1;
/* Load key modifier */
tmpdesc[idx++] = CMD_LOAD | LDST_CLASS_2_CCB | LDST_SRCDST_BYTE_KEY |
((12 << LDST_OFFSET_SHIFT) & LDST_OFFSET_MASK) |
(keymodsz & LDST_LEN_MASK);
tmpdesc[idx++] = (u32)keymod;
if(encap) {
/* Encapsulate to memory */
tmpdesc[idx++] = CMD_SEQ_IN_PTR | inbuflen;
tmpdesc[idx++] = (u32)inbuf;
}
/* Compensate for BKEK and MAC tag */
tmpdesc[idx++] = CMD_SEQ_IN_PTR | (inbuflen + CAAM_BLOB_HDR_SIZE);
if(encap) {
/* Encapsulate to memory */
tmpdesc[idx++] = (u32)outbuf;
} else {
tmpdesc[idx++] = (u32)inbuf;
tmpdesc[idx++] = CMD_SEQ_OUT_PTR | inbuflen;
tmpdesc[idx++] = (u32)outbuf;
tmpdesc[idx] = CMD_OPERATION | OP_TYPE_DECAP_PROTOCOL | OP_PCLID_BLOB |
OP_PCL_BLOB_FMT_NORMAL;
}
/* En/De-capsulate to memory */
tmpdesc[idx] = CMD_OPERATION | OP_PCLID_BLOB | OP_PCL_BLOB_FMT_NORMAL |
(encap?OP_TYPE_ENCAP_PROTOCOL:OP_TYPE_DECAP_PROTOCOL);
if (auth)
tmpdesc[idx] |= OP_PCL_BLOB_EKT;
idx++;
tmpdesc[0] = CMD_DESC_HDR | HDR_ONE | (idx & HDR_DESCLEN_MASK);
dsize = idx * sizeof(u32);
tdesc = kmalloc(dsize, GFP_KERNEL | GFP_DMA);
if (tdesc == NULL)
return 0;
memcpy(tdesc, tmpdesc, dsize);
*desc = tdesc;
return dsize;
}
What kernel version are you using? Are you running kernel in secure mode?
I am running uboot and kernel in non-secure mode. But CAAM doesn't even
create job or in simple words when i run "openssl" test for CAAM it doesn't use
CAAM driver which it should. cat /proc/crypto says
Name: cbc(aes)
driver: cbc-aes-caam
Is it same on your part?
I am using a the kernel built from a version of the Freescale 3.0.35-4.0.0 source tree. I have not done anything in particular to put the kernel itself into a "secure mode". The CPU is running signed firmware in an HAB closed configuration though.
My /proc/crypto does not show any of the caam drivers registers in the CryptoAPI. It reports:
# cat /proc/crypto
name : aes
driver : aes-generic
module : aes_generic
priority : 100
refcnt : 4
selftest : passed
type : cipher
blocksize : 16
min keysize : 16
max keysize : 32
name : arc4
driver : arc4-generic
module : arc4
priority : 0
refcnt : 3
selftest : passed
type : cipher
blocksize : 1
min keysize : 1
max keysize : 256
name : stdrng
driver : krng
module : kernel
priority : 200
refcnt : 1
selftest : passed
type : rng
seedsize : 0
name : michael_mic
driver : michael_mic-generic
module : kernel
priority : 0
refcnt : 1
selftest : passed
type : shash
blocksize : 8
digestsize : 8
I am not sure that should matter for me, as I am not trying to access the CAAM to perform generic data encryption via the CryptoAPI (i.e. openssl or ipsec), but just use the CAAM to protect a master key for use in userspace with software encryption, with the device specific OTPMK. This is what the red blobs are supposed to do, as I understand the manuals.
Sorry for the delay.
I don't remember all the details, but there is a reference implementation in the U-Boot code. The job descriptor can be understood using the Security Reference Manual and then implemented in the Linux driver.