My VPU is running at 270MHz and my Freescale FAE has said I should increase the VPU clock to 328MHz but I don't know how to. There used to be the ability in the kernel to select a config option and increase it to 352MHz (CONFIG_MX6_VPU_352M) but this has been removed from the kernel and there is no simple way to forward-port these changes to the file in question (arch/arm/mach-imx/clk-imx6q.c).
I have the latest kernel patches but it's tricky to work out exactly what to do. Please can someone help.
已解决! 转到解答。
Hi, ralph
I ported the patch to L3.10.17 for you, the patch is attached, you can refer to the patch and try to port to your code base, below is the log I tested, the VPU freq is increased, but please be noted that I did NOT do stress test on this patch, so you have to do more test on your platform, this patch is just to guide you how to increase VPU freq based n L3.10.17, it is NOT the patch that we released in our default Linux BSP! If it works for you, please close this topic, thanks!
i.MX6Q:
root@imx6qdlsolo:~# cat /sys/kernel/debug/clk/clk_summary | grep vpu
vpu_axi_sel 0 0 352000000
vpu_axi_podf 0 0 352000000
vpu_axi 0 0 352000000
root@imx6qdlsolo:~# /unit_tests/memtool 0x20c4018 1
E
Reading 0x1 count starting at address 0x020C4018
0x020C4018: 00014204
i.MX6DL:
Reading 0x1 count starting at address 0x020C4018
0x020C4018: 00A55204
root@imx6qdlsolo:~# cat /sys/kernel/debug/clk/clk_summary | grep vpu
vpu_axi_sel 0 0 327724137
vpu_axi_podf 0 0 327724137
vpu_axi 0 0 327724137
Anson (the person who wrote a patch to increase VPU frequency in the latest Yocto) has told me the repository is at ssh://sw-git01-tx30.am.freescale.net/git/sw_git/repos/linux-2.6-imx, branch: imx_3.10.y.
I don't have access to this unfortunately. Maybe it's an internal Freescale repository?
Hi, Ralph
Yes, the repository I gave you is in our internal git.
To increase the VPU freq to 328MHz on i.MX6S, you need to do some changes based on the kernel you are using, could you please tell me which kernel which release you are using?
Hi, ralph
I ported the patch to L3.10.17 for you, the patch is attached, you can refer to the patch and try to port to your code base, below is the log I tested, the VPU freq is increased, but please be noted that I did NOT do stress test on this patch, so you have to do more test on your platform, this patch is just to guide you how to increase VPU freq based n L3.10.17, it is NOT the patch that we released in our default Linux BSP! If it works for you, please close this topic, thanks!
i.MX6Q:
root@imx6qdlsolo:~# cat /sys/kernel/debug/clk/clk_summary | grep vpu
vpu_axi_sel 0 0 352000000
vpu_axi_podf 0 0 352000000
vpu_axi 0 0 352000000
root@imx6qdlsolo:~# /unit_tests/memtool 0x20c4018 1
E
Reading 0x1 count starting at address 0x020C4018
0x020C4018: 00014204
i.MX6DL:
Reading 0x1 count starting at address 0x020C4018
0x020C4018: 00A55204
root@imx6qdlsolo:~# cat /sys/kernel/debug/clk/clk_summary | grep vpu
vpu_axi_sel 0 0 327724137
vpu_axi_podf 0 0 327724137
vpu_axi 0 0 327724137
Hi Yongcai,
I applied the patch but when I select "352M" the kernel locks up on boot:
Starting kernel ...
using ft address 0x00000000
Using machid 0xEBB
uart regs:
rxd - 0x00000000
txd - 0x00000000
ctrl1 - 0x00000001
ctrl2 - 0x00004027
ctrl3 - 0x00000784
ctrl4 - 0x00008000
fifo ctrl - 0x00000200
status 1 - 0x00000240
status 2 - 0x00001000
escape char - 0x0000002B
escape timeout - 0x00000000
bpm inc - 0x0000000F
bpm mod - 0x0000015B
baud rate count - 0x00000008
one millisecond - 0x00000000
test reg - 0x00000060
485 ctrl - 0x00000000
~
When I select "328M" it boots properly and when I run "dump_clocks.sh" it tells me the VPU is now running at 328MHz. Unfortunately the effect of increasing the VPU speed is to decrease the decode frame rate to 53.6fps from 56.8fps. :-(
Is there a way to increase the IPU clock speed without increasing the VPU clock or any other clock?
Thanks,
Ralph
Hi, ralph
The 352MHz is only for i.MX6Q, 328MHz is only for i.MX6DL/S, your platfor is i.MX6S, you should only use 328MHz. I have no idea why you got decrease decode frame with high vpu freq.