Project platform information:
DSP: i.MX6DL
OS: KK4.4.2
Kernel:3.0.35
DDR:1GB
eMMC:16G
Hi FSL Guys,
According the picture above, you will find there is a around 1 second delay between the iPhone and navigation unit on CarLife. But for Android phone, the delay time is200-300 ms. Baidu guys said the long delay of iPhone may by caused by i.MX6, USB or decoder. But i cannot where i can improve. Could you advise me the possible cause?
The function SetParametor with OMX_IndexParamVideoDecReorderDisable(OMX_DECODER_REORDER) is used to disable reorder.
diff --git a/OpenMAXIL/src/component/vpu_dec_v2/VpuDecComponent.cpp b/OpenMAXIL/src/component/vpu_dec_v2/VpuDecComponent.cpp
index 2cbd9f1..29d0553 100755
--- a/OpenMAXIL/src/component/vpu_dec_v2/VpuDecComponent.cpp
+++ b/OpenMAXIL/src/component/vpu_dec_v2/VpuDecComponent.cpp
@@ -1290,7 +1290,7 @@ OMX_ERRORTYPE OpenVpu(VpuDecHandle* pOutHandle, VpuMemInfo* pInMemInfo,
{
decOpenParam.nChromaInterleave=0;
}
- decOpenParam.nReorderEnable=(bReorderDis==OMX_TRUE)?0:1; //for H264
+ decOpenParam.nReorderEnable=0; //(bReorderDis==OMX_TRUE)?0:1; //for H264
switch(eCodeFormat)
{
case VPU_V_MPEG4:
Hi Shawn
for KK4.4.2 please refer to documentation
https://www.nxp.com/webapp/Download?colCode=IMX6_KK442_100_ANDROID_DOCS
and sources
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
I cannot find the answer with your attachmnets. Could you please tell the root cause and which patch i should apply? Thank you.
In addation, this project don't have WiFi moulde. The CarLife is connected by USB cable.