I am working with the IMX50EVK and the associated daughter card MX50EBOOKDC1. This daughter card comes with a default 6 in E-ink screen which I have managed to output the linux system to. I have bought a larger E-INK screen and I want to output to this screen instead. This larger screen has a different ribbon cable. How would I be able to do this hardware wise? Are there any adapters that exist that can make this screen compatible with the daughter card?
Hi Conor
I am not aware of IMX50EVK adapters for various E-INK.
Also different Eink panel models would have different timing parameters.
So one will have to update linux epdc driver with new timing parameter table
for that E-INK screen.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------