I cannot find this package. I could find yocto_auto_linux_bsp15.0.tgz but when I build I got failure.
~/Downloads/yocto_auto_linux_bsp15.0/build_s32v234evb_release> bitbake -k fsl-image-s32v2xx
ERROR: Function failed: do_compile (log file is located at /home/wmq/Downloads/yocto_auto_linux_bsp15.0/build_s32v234evb_release/tmp/work/x86_64-linux/automake-native/1.15-r0/temp/log.do_compile.17777)
ERROR: Logfile of failure stored in: /home/wmq/Downloads/yocto_auto_linux_bsp15.0/build_s32v234evb_release/tmp/work/x86_64-linux/automake-native/1.15-r0/temp/log.do_compile.17777
Log data follows:
| DEBUG: Executing shell function do_compile
| NOTE: make -j 4
| : && /usr/bin/mkdir -p doc && { PATH='/home/wmq/Downloads/yocto_auto_linux_bsp15.0/build_s32v234evb_release/tmp/work/x86_64-linux/automake-native/1.15-r0/build/t/wrap:'$PATH && export PATH; } && /usr/bin/perl /home/wmq/Downloads/yocto_auto_linux_bsp15.0/build_s32v234evb_release/tmp/work/x86_64-linux/automake-native/1.15-r0/automake-1.15/doc/help2man --output=doc/automake-1.15.1 automake-1.15
| help2man: can't get `--help' info from automake-1.15
| Try `--no-discard-stderr' if option outputs to stderr
| make: *** [Makefile:3687: doc/automake-1.15.1] Error 255
| ERROR: oe_runmake failed
| WARNING: /home/wmq/Downloads/yocto_auto_linux_bsp15.0/build_s32v234evb_release/tmp/work/x86_64-linux/automake-native/1.15-r0/temp/run.do_compile.17777:1 exit 1 from
| exit 1
| ERROR: Function failed: do_compile (log file is located at /home/wmq/Downloads/yocto_auto_linux_bsp15.0/build_s32v234evb_release/tmp/work/x86_64-linux/automake-native/1.15-r0/temp/log.do_compile.17777)
It appears to be related to Perl but needs a patch to automake - I have no idea how to apply a patch into this build. See the link for discuss.