Hi NXP, where to find yocto_auto_linux_bsp16.0.tgz

cancel
Showing results for 
Search instead for 
Did you mean: 

Hi NXP, where to find yocto_auto_linux_bsp16.0.tgz

412 Views
David_Wu
Contributor III

I cannot find this package. I could find yocto_auto_linux_bsp15.0.tgz but when I build I got failure.

~/Downloads/yocto_auto_linux_bsp15.0/build_s32v234evb_release> bitbake -k fsl-image-s32v2xx

ERROR: Function failed: do_compile (log file is located at /home/wmq/Downloads/yocto_auto_linux_bsp15.0/build_s32v234evb_release/tmp/work/x86_64-linux/automake-native/1.15-r0/temp/log.do_compile.17777)
ERROR: Logfile of failure stored in: /home/wmq/Downloads/yocto_auto_linux_bsp15.0/build_s32v234evb_release/tmp/work/x86_64-linux/automake-native/1.15-r0/temp/log.do_compile.17777
Log data follows:
| DEBUG: Executing shell function do_compile
| NOTE: make -j 4
| : && /usr/bin/mkdir -p doc && { PATH='/home/wmq/Downloads/yocto_auto_linux_bsp15.0/build_s32v234evb_release/tmp/work/x86_64-linux/automake-native/1.15-r0/build/t/wrap:'$PATH && export PATH; } && /usr/bin/perl /home/wmq/Downloads/yocto_auto_linux_bsp15.0/build_s32v234evb_release/tmp/work/x86_64-linux/automake-native/1.15-r0/automake-1.15/doc/help2man --output=doc/automake-1.15.1 automake-1.15
| help2man: can't get `--help' info from automake-1.15
| Try `--no-discard-stderr' if option outputs to stderr
| make: *** [Makefile:3687: doc/automake-1.15.1] Error 255
| ERROR: oe_runmake failed
| WARNING: /home/wmq/Downloads/yocto_auto_linux_bsp15.0/build_s32v234evb_release/tmp/work/x86_64-linux/automake-native/1.15-r0/temp/run.do_compile.17777:1 exit 1 from
| exit 1
| ERROR: Function failed: do_compile (log file is located at /home/wmq/Downloads/yocto_auto_linux_bsp15.0/build_s32v234evb_release/tmp/work/x86_64-linux/automake-native/1.15-r0/temp/log.do_compile.17777)

It appears to be related to Perl but needs a patch to automake  - I have no idea how to apply a patch into this build. See the link for discuss.

automake 1.16 - replace Perl 'none' by tseemann · Pull Request #6352 · Linuxbrew/homebrew-core · Git... 

Labels (2)
Tags (1)
0 Kudos
1 Reply

128 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello David Nomiddlename Wu,

Are you still experiencing problems? Would you please give us more details on the BSP release you are using so we can see where the problem might reside?

Regards,

0 Kudos