Dear Sir,
My device uses a imx6 platform. I execute a "gst-launcher-1.0" command as following to convert a grey format picture file to a rgb format picture file.
gst-launch-1.0 -v filesrc location=test.grey blocksize=5038848 ! "video/x-bayer,format=bggr,width=2592,height=1944,framerate=1/1" ! bayer2rgb ! filesink location=test.rgb
Most of time, this command executes successfully to convert my file "test.grey" to my desired file "test.rgb". However an error occurs randomly and the error is shown below:
Caught SIGSEGV
#0 0x76be71a4 in poll () at ../sysdeps/unix/syscall-template.S:84
#1 0x76ccccb4 in ?? () from /usr/lib/libglib-2.0.so.0
Spinning. Please run 'gdb gst-launch-1.0 15629' to continue debugging, Ctrl-C to quit, or Ctrl-\ to dump core.
After diving into the source files, I found this error results from the function "bin_handle_async_done()" in the gstream source file "gstbin.c".
My question is : why this error occurs? Because I have seen the error several times on different testing scenarios. I executed a test script to execute this command for 2000 times and this error always occurs at different loop. Sometimes it occurs at 220th loop and next time it occurs at 515th loop or 858th loop. In brief, this error occurs randomly.
Does anyone have similar problem as I do?
Please help,
Thanks,
Peter
Dear Igor,
Here is the url where I post my question in github for your reference.
Thanks,
Peter
Dear Carlos,
Got it. Because this is my first time posting a message here and am not familiar with the procedures, that's why there are three duplicated threads. I am sorry about it. And I am looking forward to the answer from your team.
Thanks a lot,
Peter
Hi Peter
may be suggested to open issue on gstreamer-imx github page
https://github.com/Freescale/gstreamer-imx/issues
Best regards
igor
Hi peter,
this thread is duplicated with the following threads:
Help: an SIGSEGV error in gst-launch-1.0 (v 1.8.1) (thread/477845)
Help: an SIGSEGV error in gst-launch-1.0 (v 1.8.1) (thread/477846)
Help: an SIGSEGV error in gst-launch-1.0 (v 1.8.1) (thread/477847)
I will close the others and only keep this.
Somebody in our team will anwer your question.
Regards,
Carlos