I'm trying to boot a custom board from NFS with no success, it get stucked when init memory is freed.
I fallowed the intructions from Android_User_Guide.pdf. I don't see any error output.
Can someone give a hint on this issue?
I attached the log file to show command line, etc.
....
ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
Sending DHCP requests ., OK
IP-Config: Got DHCP answer from 0.0.0.0, my address is 192.168.1.38
IP-Config: Complete:
device=eth0, addr=192.168.1.38, mask=255.255.255.0, gw=192.168.1.1,
host=192.168.1.38, domain=imagikcorp.local, nis-domain=(none),
bootserver=0.0.0.0, rootserver=192.168.1.35, rootpath=
VFS: Mounted root (nfs filesystem) on device 0:12.
Freeing init memory: 236K
Original Attachment has been moved to: android_log.txt.zip
Yamil
This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.
Thanks,
Yixing
Yamil
We have not got your response yet and will close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.
Thanks,
Yixing
Yamil
We are sorry for getting back to you so late. Are you still stuck with the issue? If you have somehow to resolved the issue, can we close the discussion? If you still need Freescale help, please feel free to contact us.
Thanks,
Yixing