Hello everyone, following the discussion here, I was able to get wifi running.
And I was wondering if anyone has succeeded in getting bluetooth to work in Jellybean.
I will begin working on this tomorrow, and I will post all my findings here. Hope you can do the same.
Thank you!
If you required ,you can send to me your private mail. I can share all bluetooth vendor implement with you.
All my source code is open sourced on xhteam · GitHub
You can find bluetooth relevant code in
hardware-imx/wlan/marvell at hostpadfix · xhteam/hardware-imx · GitHub
and
device-common/libbt-mrvl at imx_jb · xhteam/device-common · GitHub
Hope this can help you.
Hi, I used Marvel SD8782 module (88W8782-NAP2).
Is it compatible with 8787 driver and firmware(sd8787_uapsta.bin)?
Because I don't find any driver and firmware named "sd8782".
Thanks a lot!!
I know nothing about 8782,please contact Marvell partner.
Hi , we now have AOSP running the galaxy tab 3 7in I would like to also recieve bt source android.c357@gmail.com
Check your mailbox! I think everything your need attached.
Hello Raymond
using the correct drivers I manage to use the bluetooth port (/dev/mbtchar0) using bdt (bluedroid test tool)
however when I try to activate bluetooth using settings-->bluetooth GUI I receive the following errors on logcat:
E/BluetoothAdapter(: Bluetooth binder is null
E/DeviceListPreferenceFragment: Bluetooth is not supported on this device
so apparently bludroid works fine with my definitions but GUI will not , any idea?
* I have already added
device.mk
# Bluetooth
PRODUCT_COPY_FILES += \
frameworks/native/data/etc/android.hardware.bluetooth.xml:system/etc/permissions/android.hardware.bluetooth.xml
Please start a new thread for your issue. And more technical details required for your issue. e.g.
More logcat of bluetooth service. Paste your ps output and find out if proccess com.android.bluetooth
existed.
Hello Raymond
can you please send me the all SD8787 WIFI + Bluetooth needed files ?
thank you!
Hi, Raymond ! Could you share the vendor stack with me too ?
I'm bringing up sd8787-based bluetooth in JB 4.3, and these pieces is just was I miss.
Thanks !
Andrey [segfalta@gmail.com]
Check your mailbox! I think everything your needed was attached.
Thanks very much, your help is invaluable !
I would like to point out, that MarvellWirelessDaemon / libMarvellWireless are actually optional (having role much resembling that of wifi.c), and can quite safely be left out.
Hi Raymond, I am also trying to enable bt on sd8787 after integrating the driver. i am getting below error
E/bt-btif ( 45): ...preload_wait_timeout (retried:0/max-retry:0)
I am still using default athros lib-vendor library, Can your please share your vendor implement for bluedroid stack?
It will be really helpful for me.
my private mail id is riteshraj21@gmail.com
Hi Raymond, we are using the same module for our customized imx6 board, we didn't use Marvell's libbt-vendor.so for the bt module, instead we ported 'Bluez+bt8xxx.c' to replace the original 'Bluedroid+char device' for Android 4.2.2. We almost get there, but we always encounter a timeout issue while bring up the BT module. The error message list as belows: BT: module_cfg_cmd (0xf1): timeout sendcmdflag=1, and then the BT won't bring up. It must happen after several times of BT off-on status reversed. Once it happened, nothing but reboot can bring up the BT module again. So, have you ever encountered such timeout issue? What about the current status of your stacks porting? My mail address is 'xj.gan@vantrontech.com', I am expecting a further discuss with you about the Marvell BT issue, thanks!