Has anyone built the mainstream U-boot and gotten it to boot the freescale provided kernel?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Has anyone built the mainstream U-boot and gotten it to boot the freescale provided kernel?

997件の閲覧回数
blsousan
Contributor III

All,

     I need additional U-boot features than the ones provided in the freescale version of U-boot.  I have got the latest U-boot source and compiled it for the iMX28evk.  The new U-boot seems to work fine.  However, when it goes to start the kernel I just get:

Uncompressing kernel... done,  booting the kernel.

And nothing else.  I'm using the same kernel with both the original Uboot from freescale and the one I just built.  The original U-boot boots it just fine.

Thanks,

Bills

ラベル(1)
0 件の賞賛
4 返答(返信)

819件の閲覧回数
OtavioSalvador
Senior Contributor II

We've been using mx28evk with  Yocto, with mainline u-boot, for quite sometime ... so it really seem to be the console. Check the whole env as you might be using the wrong bootargs.

0 件の賞賛

819件の閲覧回数
OtavioSalvador
Senior Contributor II

You need to use ttyAM for default FSL kernel and ttyAMA for mainline. You seem to use FSL kernel so change console variable.

0 件の賞賛

819件の閲覧回数
blsousan
Contributor III

Thanks.  Yes I tried that previously (using ttyAMA0 - found it in another post) and it did not make a difference.  I'm not sure about using the mainline Linux kernel.  I was referring to the mainline U-boot with the existing kernel.  However, I may try it with a mainline Kernel (just hope this does not  "ripple" through and end up needed to upgrade a bunch of packages)

Thanks,

Bills

0 件の賞賛

819件の閲覧回数
ThomasWaldecker
Contributor I

Hi Bills,

you need to change the console for Linux from console=ttyAM0,115200 to console=ttyAMA0,115200

Also note the wiki page at: http://imxdev.org/wiki/index.php?title=Running_a_mainline_kernel_on_a_MX28EVK_board

(easily found with google)

Kind regards,

Thomas

0 件の賞賛