Hardware VPU decoder for firefox

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hardware VPU decoder for firefox

3,825 Views
zhencongtee
Contributor III

Greetings,

May i know how can I integrate the VPU decoder into the firefox brower?

I am using Yocto build on i.MX6q SabreSD board.

I manage to integrate the firefox browser in the image already. But when i wanted to run some video in the browser, it is not supported.

When i run the below page:

http://www.youtube.com/html5

The h.264 and VP8 is not ticked.

I am able to run h.264 and VP8 video in gstreamer. Just that i have no idea how can i like the gstreamer to be used in firefox? Or it cannot be done at all?

Anybody has any idea on this issue?

Thanks.

Regards,

Zhen Cong Tee

0 Kudos
Reply
3 Replies

2,899 Views
igorpadykov
NXP Employee
NXP Employee

Hi Zhen

please check below, seems this is what you are looking for

Porting Chrome on i.mx6 with hw accelaration?

OSSystems/meta-browser · GitHub

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,899 Views
zhencongtee
Contributor III

Hi Chip,

The page does not mentioning about integrating VPU into the browser.

I did a little background survey on firefox, and from page below:

http://en.wikipedia.org/wiki/History_of_Firefox

I found out that firefox only support gstreamer starting version 14.

From the meta-browser, the firefox version that is available in yocto is 10.0.11esr.

May i know how can i upgrade the yocto firefox to version 14 to test out the gstreamer?

Thank you.

Regards,

Zhen Cong Tee

2,899 Views
igorpadykov
NXP Employee
NXP Employee

Hi Zhen

Please post this question

to meta-fsl-arm mailing list, so that someone familiar with integrating VPU

to firefox could try to assist you.

https://lists.yoctoproject.org/listinfo/meta-freescale

Best regards

chip

0 Kudos
Reply