HDMI hotplug not working in iMX7D Sabresd.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HDMI hotplug not working in iMX7D Sabresd.

761 Views
deven_solanki
Contributor III

Hi ,

I am working on imx7d-sabresd board. and I am using NXP i.MX Release Distro 4.9.11-1.0.0 (morty). I am facing issue with HDMI hard plugged in. If I plugged in HDMI cable at the booting time itself then I am getting output on HDMI display. But if I am booting board without plugged in HDMI cable and after complete boot I plugged in HDMI cable then it is not giving any output.

How to resolve this problem?

Thanks in advance

Deven Solanki

Labels (1)
Tags (1)
0 Kudos
1 Reply

369 Views
igorpadykov
NXP Employee
NXP Employee

Hi Deven

one can try to debug it checking with oscilloscope signal HDMI_INT_B iI9022A

change on GPIO_EPDC_D13 (MX7D_PAD_EPDC_DATA13__GPIO2_IO13)

 p.6 spf-28590 i.MX7D SabreSD schematic

Schematics (2)
Design files for i.MX 7Dual (REV D)
Design files, including hardware schematics, Gerbers, and OrCAD files for i.MX 7Dual (REV D)
http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

check with corresponding linux/arch/arm/boot/dts/imx7d-sdb.dts

linux-imx.git - i.MX Linux Kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos