root@imx8mp-lpddr4-evk:~# paprefs
(paprefs:1751): Gtk-WARNING **: 09:53:52.943: Could not load a pixbuf from /org/gtk/libgtk/theme/Adwaita/assets/bullet-symbolic.svg.
This may indicate that pixbuf loaders or the mime database could not be found.
root@imx8mp-lpddr4-evk:~# pavucontrol
(pavucontrol:1772): Gtk-WARNING **: 09:54:09.895: Could not load a pixbuf from /org/gtk/libgtk/theme/Adwaita/assets/check-symbolic.svg.
This may indicate that pixbuf loaders or the mime database could not be found.
How to fix this warning "trying to set for simultaneous audio play" but i am not able to get that option. Assist me to get that option (or) any alternative solution to get dual Bluetooth play on two paired headset.
root@imx8mp-lpddr4-evk:~# pactl list short modules
0 module-device-restore
1 module-stream-restore
2 module-card-restore
3 module-augment-properties
4 module-switch-on-port-available
5 module-udev-detect tsched=0
6 module-alsa-card device_id="0" name="platform-sound-bt-sco" card_name="alsa_card.platform-sound-bt-sco" namereg_fail=false tsched=no fixed_latency_range=no ignore_dB=no deferred_volume=yes use_uc"
7 module-alsa-card device_id="1" name="platform-sound-hdmi" card_name="alsa_card.platform-sound-hdmi" namereg_fail=false tsched=no fixed_latency_range=no ignore_dB=no deferred_volume=yes use_ucm=ye"
8 module-alsa-card device_id="2" name="platform-sound-micfil" card_name="alsa_card.platform-sound-micfil" namereg_fail=false tsched=no fixed_latency_range=no ignore_dB=no deferred_volume=yes use_uc"
9 module-alsa-card device_id="3" name="platform-sound-xcvr" card_name="alsa_card.platform-sound-xcvr" namereg_fail=false tsched=no fixed_latency_range=no ignore_dB=no deferred_volume=yes use_ucm=ye"
10 module-bluetooth-policy
11 module-bluetooth-discover headset=auto
12 module-bluez5-discover headset=auto
13 module-native-protocol-unix
14 module-default-device-restore
16 module-always-sink
17 module-intended-roles
18 module-suspend-on-idle
19 module-systemd-login
20 module-position-event-sounds
21 module-role-cork
22 module-filter-heuristics
23 module-filter-apply
25 module-null-sink sink_name=virtual_combined_sink
26 module-bluez5-device path=/org/bluez/hci0/dev_01_A2_00_12_FC_DD autodetect_mtu=0 output_rate_refresh_interval_ms=500 avrcp_absolute_volume=1
27 module-bluez5-device path=/org/bluez/hci0/dev_11_11_22_39_23_1A autodetect_mtu=0 output_rate_refresh_interval_ms=500 avrcp_absolute_volume=1
"In the above i am not able to get module-combine-sink" Even though i have copied the module-combine-sink and configured in /etc/pulse/default.pa " load-module module-alsa-source device=combined
load-module module-null-sink sink_name=virtual_combined_sink "
but still not able to play on two Bluetooth paired devices.
Does this IMX8m Plus Evk broad with Azure Wave BT/Wifi supports for dual audio play on two paired Bluetooth devices?
Hello @joanxie
Is there way, that can we make output audio to play simultaneously one from headphone jack (Earphone plugin)given on the Imx8m evk and another from Bluetooth paired (Bluetooth earphones) devices from single source (audio).
If there is way, please guide.
Because in my yocto build image(imx-image-full), pulseaudio doesn't contain module-combine-sink even though i have updated version of pusleaudio 16.1, Detail's below,
I suggest that you can create a new thread for this feature request, and put them to the wireless group, not imx group, attach your detailed request, they will give you more detailed answer for how to support such feature, because current bsp doesn't support this, you need double confirm from them,