We are trying Sabre Lite (i.MX6Q) with provided Ubuntu image (3.0.35_4.1.0 kernel), connected to HDTV with HDMI, 1920x1080@60,if=RGB24.
Gstreamer pipeline we used is simple and its reproducible with h264 or mpeg2 videos (probably any video but we didn't test others).
gst-launch-0.10 filesrc location=path/to/file typefind=true ! aiurdemux ! queue max-size-time=0 max-size-buffers=0 ! vpudec ! mfw_v4lsink
I've taken photos that show the problem and attached them. Please notice background color gradient and ignore bad photo quality as it was taken by phone.
Best description would be that video sink has poor color depth, there is effect of color banding.
Same video, when played on PC, doesn't have such issues.
We have tired to find root of the problem, as for now we have managed to conclude that it is not display or decoder problem:
We have tested 3 different TV models and one monitor, and all display same issue.
We have dumped raw video (after decoder) to file and played it on PC, there where no such issues.
While writing this, we have added bpp=32 to 1920x1080@60,if=RGB24 boot arguments and it looks a better, but still not good as same video displayed on PC monitor or TV decoder.
That might lead us to root of the problem.
Also, there are topics that touched this problem but never received proper answers:
Color banding in video using mfw_isink with GStreamer
Any ideas?
已解决! 转到解答。
Hi David and Karina,
This is an old issue and it would really be nice to get the fixes up-streamed.
https://community.freescale.com/thread/220507
The short answer is that you're seeing the default alpha-blending of the video overlay. Notice the text bleeding through the video in Photo 1.
We have patches floating around, but didn't apply them when we built the image above. On that image, we didn't apply the patches. We simply used the Freescale-supplied binaries.
We have a newer image that contains the latest gstreamer plugins here, but we also didn't apply the patches here:
http://boundarydevices.com/rapping-raring/
Note that the patches aren't really needed when you're using your own application, since you can call the FB ioctls directly to configure color-keying and blending levels for the YUV overlay.
EricNelson can you help on this case?
Hi David and Karina,
This is an old issue and it would really be nice to get the fixes up-streamed.
https://community.freescale.com/thread/220507
The short answer is that you're seeing the default alpha-blending of the video overlay. Notice the text bleeding through the video in Photo 1.
We have patches floating around, but didn't apply them when we built the image above. On that image, we didn't apply the patches. We simply used the Freescale-supplied binaries.
We have a newer image that contains the latest gstreamer plugins here, but we also didn't apply the patches here:
http://boundarydevices.com/rapping-raring/
Note that the patches aren't really needed when you're using your own application, since you can call the FB ioctls directly to configure color-keying and blending levels for the YUV overlay.