Gstreamer plugin to have reduced latency in streaming

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Gstreamer plugin to have reduced latency in streaming

1,479 Views
snehal_jadhav
Contributor III

Hi,

We are streaming camera from imx6q platform on remote display which has NVIDIA GPU. We are using below gstreamer pipeline on remote display to stream camera. In below pipeline we are using NVIDIA decoder plugin.

gst-launch-1.0 -e -v udpsrc port=5000 ! application/x-rtp,encoding-name=H264,payload=96 ! rtpjitterbuffer latency=0 drop-on-latency=TRUE ! rtph264depay ! video/x-h264 ! h264parse ! nvdec ! glimagesink sync=false

with this pipeline we are getting ~116ms to ~175ms latency in camera streaming on remote display. How we can reduce our latency in video streaming. Is there any gstreamer plugin which can help us reduce latency or any other way.

Thanks

Labels (1)
Tags (3)
0 Kudos
Reply
1 Reply

1,163 Views
Dhruvit
NXP TechSupport
NXP TechSupport

Hi,

I am exploring the issue, and below are the details required for further analysis to debug this issue. Can you please help me with the same?

  1. Can you please provide me with the command which you are firing at the processor side?
  2. Through which medium the camera data is sent to the remote display?

 

Best Regards,

Dhruvit.

0 Kudos
Reply