Hi All,
I am trying to cross compile the gstreamer-0.10.25 for arm I do the following
/configure --prefix=/home/sarahblessie/gstlib/ CC=arm-linux-gnueabi-gcc CXX=arm-linux-gnueabi-g++ --host=arm-linux LDFLAGS=-L/home/sarahblessie/gstlib/lib CFLAGS=-I/home/sarahblessie/gstlib/include --build=i686-linux
when I give make I get following error
Making all in pkgconfig
Making all in gst
Making all in parse
CC lex._gst_parse_yy.o
CC grammar.tab.o
LINK libgstparse.la
CC gst.o
CC gstobject.o
CC gstbin.o
CC gstbuffer.o
CC gstbufferlist.o
CC gstbus.o
CC gstcaps.o
CC gstchildproxy.o
CC gstclock.o
CC gstdebugutils.o
CC gstelement.o
gstelement.c: In function ‘gst_element_get_request_pad’:
gstelement.c:1017:8: warning: variable ‘n’ set but not used [-Wunused-but-set-variable]
CC gstelementfactory.o
gstelementfactory.c: In function ‘gst_element_factory_create’:
gstelementfactory.c:419:1: error: size of array ‘_GStaticAssertCompileTimeAssertion_3’ is negative
gstelementfactory.c:418:3: error: invalid use of void expression
gstelementfactory.c:418:3: error: incompatible type for argument 1 of ‘__sync_bool_compare_and_swap’
make[4]: *** [libgstreamer_0.10_la-gstelementfactory.lo] Error 1
make[3]: *** [all-recursive] Error 1
make[2]: *** [all] Error 2
make[1]: *** [all-recursive] Error 1
make: *** [all] Error 2
Please give me some solution, Thanks in advance
Regards,
Sarah
why don' t you use freescale bsp? which includes corss compilation for arm, the old version is linux3.0.101. the latest version is 3.10.53
I have a vayu evm board and trying to compile it for the board