Gic-v3 Interrupt being blocked on ATF version imx_4.14.98_2.0.0_ga

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Gic-v3 Interrupt being blocked on ATF version imx_4.14.98_2.0.0_ga

1,587 Views
hafizabdul_kari
Contributor III

I am running Multicore Framework in AMP configuration on A-53 cores i.e. Linux master on 1st two core and an RTOS (slave) on the other two.

Interrupts are being generated and received properly when ATF version imx_4.14.78_1.0.0_ga is used. but when we move to ATF version imx_4.14.98_2.0.0_ga the interrupts are being generated from RTOS but somehow are not received on linux side.

5 Replies

1,379 Views
hafizabdul_kari
Contributor III

Hi Igor,

Thanks for your kind help.

Actually when we use same versions of all the components (u-boot, atf, kernel ) i.e. 4.14.98  , we get this issue.

But if we use 4.14.78 version of atf with 4.14.98 version of u-boot and kernel,  things work fine.

Best Regards,

Abdul Karim.

0 Kudos

1,380 Views
igorpadykov
NXP Employee
NXP Employee

Hi Abdul

 

this may point that you are using old silicon version.

 

Best regards
igor

1,380 Views
hafizabdul_kari
Contributor III

Hi Igor,

My silicone rev is B3, Can you please confirm if SDK 4.14.98  is applicable to this revision?

Best Regards,

Abdul Karim

0 Kudos

1,380 Views
igorpadykov
NXP Employee
NXP Employee

Hi Abdul 

there is no i.MX8QM processor with "silicone rev is B3".

Also since this part is "PRE-PRODUCTION" as described on link

i.MX 8 Family Applications Processor | Arm Cortex-A53/A72/M4 | NXP 

it has not full support. Suggest to proceed with help of Commercial Support and Engineering Services | NXP 

Best regards
igor

0 Kudos

1,380 Views
igorpadykov
NXP Employee
NXP Employee

Hi Abdul

issue may be related to version dependency: that is linux version,

scfw version and atf version should be used all as 4.14.98 and not mixed

with 4.14.78 or other versions. Please refer to below link for available patches and scfw revisions:

i.MX Software | NXP 

Please also be aware of software dependancy for chip revision

("Production" vs "Samples" and 1.7v refgen) and pmic revision (C1).

Suggest to apply to local marketing office to get more details.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos