Hi, I'm using the Sabre-SD board with the rootfs from L3.0.35_4.1.0_DEMO_IMAGE_BSP.
I am having trouble getting the audio to work over HDMI (video works).
Resolution is set to video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24
aplay -l also shows both audio devices.
root@freescale ~$ aplay -l
**** List of PLAYBACK Hardware Devices ****
card 0: wm8962audio [wm8962-audio], device 0: HiFi wm8962-0 []
Subdevices: 1/1
Subdevice #0: subdevice #0
card 1: imxhdmisoc [imx-hdmi-soc], device 0: IMX HDMI TX mxc-hdmi-soc-0 []
Subdevices: 1/1
Subdevice #0: subdevice #0
Running speaker-test -Dplughw:0, there is audio coming out of the headphone jack.
Similarly, aplay also works.
root@freescale ~$ cat /dev/urandom | aplay -Dplughw:0
Playing raw data 'stdin' : Unsigned 8 bit, Rate 8000 Hz, Mono
However, when I run speaker-test -Dplughw:1 or cat /dev/urandom | aplay -Dplughw:1
it doesn't give any error, but there is no sound coming out.
root@freescale ~$ cat /dev/urandom | aplay -Dplughw:1
Playing raw data 'stdin' : Unsigned 8 bit, Rate 8000 Hz, Mono
Are any special settings needed for configuring the audio to output to HDMI ? Any help is appreciated. Thanks!
Alex
We are sorry for getting back to you so late. Are you still stuck with the issue? If you have somehow to resolved the issue, can we close the discussion? If you still need help, please feel free to reply with an update to this discussion.
Thanks,
Yixing