Getting HDMI audio to work on sabre-sd

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Getting HDMI audio to work on sabre-sd

1,186 Views
alexhe
Contributor I

Hi, I'm using the Sabre-SD board with the rootfs from L3.0.35_4.1.0_DEMO_IMAGE_BSP.

I am having trouble getting the audio to work over HDMI (video works).

Resolution is set to video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24

aplay -l also shows both audio devices.

root@freescale ~$ aplay -l

**** List of PLAYBACK Hardware Devices ****

card 0: wm8962audio [wm8962-audio], device 0: HiFi wm8962-0 []

  Subdevices: 1/1

  Subdevice #0: subdevice #0

card 1: imxhdmisoc [imx-hdmi-soc], device 0: IMX HDMI TX mxc-hdmi-soc-0 []

  Subdevices: 1/1

  Subdevice #0: subdevice #0

Running speaker-test -Dplughw:0, there is audio coming out of the headphone jack.

Similarly,  aplay also works.

root@freescale ~$ cat /dev/urandom | aplay -Dplughw:0

Playing raw data 'stdin' : Unsigned 8 bit, Rate 8000 Hz, Mono

However, when I run speaker-test -Dplughw:1 or cat /dev/urandom | aplay -Dplughw:1

it doesn't give any error, but there is no sound coming out.

root@freescale ~$ cat /dev/urandom | aplay -Dplughw:1

Playing raw data 'stdin' : Unsigned 8 bit, Rate 8000 Hz, Mono

Are any special settings needed for configuring the audio to output to HDMI ? Any help is appreciated. Thanks!

Labels (4)
Tags (4)
0 Kudos
4 Replies

572 Views
YixingKong
Senior Contributor IV

Alex

This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.

Thanks,

Yixing

0 Kudos

572 Views
puneetpalsingh
NXP Employee
NXP Employee

I am facing this same issue.
Can somebody help?

0 Kudos

572 Views
YixingKong
Senior Contributor IV

Alex

We have not got your response yet and will close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 Kudos

572 Views
YixingKong
Senior Contributor IV

Alex

We are sorry for getting back to you so late. Are you still stuck with the issue? If you have somehow to resolved the issue, can we close the discussion? If you still need help, please feel free to reply with an update to this discussion.

Thanks,
Yixing

0 Kudos