GT928 configuration with IMX8MM board in A11 code

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GT928 configuration with IMX8MM board in A11 code

341 Views
divyeshmarne0
Contributor III

 

Hi Team,

We are integrating touch controller GT928 with imx8mm in Android 11 code base.

We need confirmation on following two points:

1. Can you provide I2C Register address for gt928.

2. Apart from DTSI changes, what are the changes required to configure I2C slave address?

 As per data sheet GT928 supports two I2C slave addresses: 0xBA/0xBB and 0x28/0x29. The host can select the address by changing the status of Reset and INT pins during the power-on initialization phase".

For power-on initialization phase, Do we need to make any changes in driver or DTSI changes would be enough ?

Thnaks

Divyesh

0 Kudos
0 Replies