[I.MX8MQ-EVK] for secure boot.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[I.MX8MQ-EVK] for secure boot.

986件の閲覧回数
Ashoka_A_D
Contributor I

Hi All,

I have i.mx8mq-evk board, i want to start the secure boot in it. any body can help me to do this from scratch.? 

i have  few doubts.

1. can i able to do the secure boot in this board.?

2. Is OTP is present on the board.?

 

Advance thanks for your response.

0 件の賞賛
返信
2 返答(返信)

970件の閲覧回数
frix
Contributor II

Just a heads up - if you proceed to encrypted boot, there's a typo in mx8m_encrypted_boot.txt:

Line 454:   MAC offset = csf_fit_enc.bin size - Nonce/MAC size
Line 455:                      = 4020 - 36 = 3984 Byte

The file referenced, should be 'csf_fit_sign_enc.txt', not 'csf_fit_enc.bin'. The size in line 455: 4020 bytes are however correct.

0 件の賞賛
返信

982件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信