I am trying to get the SABRE Lite board working with my parallel camera (OV5642 based Nit6X_5MP module), both from Boundary Devices:
http://boundarydevices.com/product/nit6x_5mp/
I am running the Yocto Dizzy pre-built image from Boundary Devices which boots up fine.
I was trying to get the camera input to be displayed on the HDMI monitor, but it consistently fails. The "ov5642_camera" and "mxc_v4l2_capture" modules are loaded per the console:
Module Size Used by
bluetooth 194905 2
ov5642_camera 122025 0
ov5640_camera_mipi 52395 0
mxc_v4l2_capture 24905 3 ov5642_camera,ov5640_camera_mipi
ipu_bg_overlay_sdc 4175 1 mxc_v4l2_capture
ov5640_camera 18199 0
ipu_still 1719 1 mxc_v4l2_capture
ipu_prp_enc 4707 1 mxc_v4l2_capture
adv7180_tvin 7304 0
ipu_csi_enc 2969 1 mxc_v4l2_capture
ipu_fg_overlay_sdc 5051 1 mxc_v4l2_capture
v4l2_int_device 1796 5 ov5642_camera,ov5640_camera_mipi,adv7180_tvin,mxc_v4l2_capture,ov5640_camera
flexcan 8689 0
can_dev 6641 1 flexcan
My Gstreamer command is as simple as it gets:
gst-launch mfw_v4lsrc ! mfw_v4lsink
but as the console shows, it fails with the error "ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0".
root@nitrogen6x:~# gst-launch mfw_v4lsrc ! mfw_v4lsink
MFW_GST_V4LSRC_PLUGIN 3.0.11 build on Nov 7 2014 14:00:20.
mxc_v4l_open: Mxc Camera no sensor ipu1/csi0
mxc_v4l_open: Mxc Camera no sensor ipu1/csi1
MFW_GST_V4LSINK_PLUGIN 3.0.11 build on Nov 7 2014 14:00:16.
Setting pipeline to PAUSED ...
Pipeline is live and does not need PREROLL ...
Setting pipeline to PLAYING ...
New clock: GstSystemClock
ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0
ERROR: from element /GstPipeline:pipeline0/MFWGstV4LSrc:mfwgstv4lsrc0: Internal data flow error.
Additional debug info:
/home/ericn/yocto18/build-nitrogen6x/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/gstreamer/0.10.36-r2/gstreamer-0.10.36/libs/gst/base/gstbasesrc.c(2625): gst_base_src_loop (): /GstPipeline:pipeline0/MFWGstV4LSrc:mfwgstv4lsrc0:
streaming task paused, reason error (-5)
Execution ended after 10004338334 ns.
Setting pipeline to PAUSED ...
Setting pipeline to READY ...
Setting pipeline to NULL ...
Total rendered:0
Freeing pipeline ...
[--->FINALIZE v4l_sink
root@nitrogen6x:~# power_down_callback: ipu0/csi0
The behavior changes if I specify "capture-mode=5" or "capture-mode=6", but it fails with a different error.
root@nitrogen6x:~# gst-launch mfw_v4lsrc capture-mode=6 ! mfw_v4lsink
MFW_GST_V4LSRC_PLUGIN 3.0.11 build on Nov 7 2014 14:00:20.
mxc_v4l_open: Mxc Camera no sensor ipu1/csi0
mxc_v4l_open: Mxc Camera no sensor ipu1/csi1
MFW_GST_V4LSINK_PLUGIN 3.0.11 build on Nov 7 2014 14:00:16.
Setting pipeline to PAUSED ...
mxc_v4l2_s_param: vidioc_int_s_parm returned an error -22
ERROR: Pipeline doesn't want to pause.
Setting pipeline to NULL ...
Total rendered:0
Freeing pipeline ...
[--->FINALIZE v4l_sink
Any hints of where to look for the trouble would be appreciated!
Hi,
has this issue been solved ? If yes, i have same issue, every feedback would be helpful.