Hello!
I am trying to get android gps system working. I have a gps module
which output NMEA format data. It is connected to my devboard through
USB and I use standard ftdi driver. It creates /dev/ttyUSB0 interface.
Output speed of gps data is 4800, I change to it with busybox stty -F /
dev/ttyUSB0 4800 from 115200. I downloaded freerunner nmea gps parser
that implements gps.h. Then i put the source file (fr_gps.c) of parser
to
$android/src/hardware/mx5x/libgps/
directory with Android.mk file
LOCAL_PATH := $(call my-dir)
ifneq ($(TARGET_PRODUCT),sim)
# HAL module implemenation, not prelinked and stored in
# hw/<GPS_HARDWARE_MODULE_ID>.<ro.hardware>.so
include $(CLEAR_VARS)
LOCAL_PRELINK_MODULE := false
LOCAL_MODULE_PATH := $(TARGET_OUT_SHARED_LIBRARIES)/hw
LOCAL_SHARED_LIBRARIES := liblog libcutils libhardware
LOCAL_SRC_FILES := gps_freerunner.c
#LOCAL_SRC_FILES += gps.c
LOCAL_MODULE := gps.default
LOCAL_MODULE_TAGS := eng
include $(BUILD_SHARED_LIBRARY)
# endif
endif
after compilation i put gps.default.so to
/system/lib/hw
directory and reboot my android. But any map application shows "GPS
disabled couldnt get location".
I didnt set BOARD_GPS_LIBRARIES in BoardConfig.mk. greping all files
in source tree I didnt find any file that using it. In source file of
parser I see LOGD messages but logcat didnt show anything. Could
anybody put me on right way, give some advices? googling through web
gives me fractional information about this.
Thanks!
Hi,
I have similar problem. My GPS device is on /dev/ttyUSB3, i see output with "cat /dev/ttyUSB3"
I added freerunner driver, and changed BoardConfig adding:
BOARD_GPS_LIBRARIES := libgps
Also i added entry in init.rc:
setprop ro.kernel.android.gps ttyUSB3
But GPS is not working in Android.
Can you help me?
Best regards,
Toxic
Hello,
I have changed LOCAL_MODULE := gps.default to LOCAL_MODULE := gps.<platform> and GPS almost works.
Only problem i have at the moment is incorrect number of sattelites.
I suppose that fix is here: NelsonChung's blog: Android GPS porting HAL code - Fix GPSStatus and GPSSvStatus issue.
Could someone translate (explain) it for me? I don't know Chineese language.
Best regards,
Toxic
Hi kirill, can u send me how u got it working even im facing the same problem, i got data in the terminal when doing cat /dev/ttyUSB0, i did the same thing like you with freerunner implementation.
Can u help me please.
Kirill Danilenko said:
Thanks for reply, I already get it working.
Hello Kiril,
I am at exactly the same point as you have described.
Apparently, my gps.imx5x.so file does not contain symbol "HMI" , the error spat on logcat:
E/HAL ( 2223): load: couldn't find symbol HMI
The Android.mk file looks 95% identical to yours, the only difference is that I am building the .so under hardware/mygpssupport instead of hardware/mx5/mygps....
How could I make HMI appear in the file, so code execution could proceed in hardware/libhardware/hardware.c:163:
hmi = (struct hw_module_t *)dlsym(handle, sym);
Many thanks,
Simonas
Hi Kirill,
I am using customized board based on am335xevm , and i have ported linux and android
I am new to android , but have managed to read the gps data on linux (by opening and read the uart port data)
I need to add android gps driver (in order to make the gps chip communicate with GL engine and Android Location Services)
Kindly ,would you give me some advices and guidelines to make do that.
thanks
Carl
here are some notes from the one makes gps working on imx51_bbg:
http://nelsonchunglife.blogspot.com/2010/12/android-gps-porting-hal-code-fix.html