Hi,
My query was marked as spam : https://community.nxp.com/t5/i-MX-Processors/GPIO5-IO26-IRQ-issue-in-i-MX8MM-EVK-HW/m-p/1261756#M172...
so, I am reposting again with different title.
My Query starts:
-----------------------
I am working with i.mx8mm evk hw and yocto distribution 4.19 warrior version.
My application requires rising edge sensitive interrupt, so i need to use gpio pins instead of EXP_IO interrupt (which is giving level sensitive interrupts). so i choosed UART3_RxD / GPIO5_IO26 pin for my IRQ
I am trying to use GPIO5_IO26 for IRQ operation, uart3_rxd pad is muxed with gpio5_io26.
I made the below changes in the dts file.
my_irq_pin: my_irq_pin {
compatible = "my_drv";
interrupt-parent = <&gpio5>;
interrupts = <26 IRQ_TYPE_EDGE_RISING>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_myirq_pin>;
status = "okay";
};
&iomuxc {
pinctrl-names = "default";
..................
imx8mm-evk {
pinctrl_myirq_pin: myirq_pin {
fsl,pins = <
MX8MM_IOMUXC_UART3_RXD_GPIO5_IO26 0x16
>
};
pinctrl_uart1: uart1grp {
fsl,pins = <
MX8MM_IOMUXC_UART1_RXD_UART1_DCE_RX 0x140
MX8MM_IOMUXC_UART1_TXD_UART1_DCE_TX 0x140
/*MX8MM_IOMUXC_UART3_RXD_UART1_DCE_CTS_B 0x140 */
MX8MM_IOMUXC_UART3_TXD_UART1_DCE_RTS_B 0x140
MX8MM_IOMUXC_SD1_DATA4_GPIO2_IO6 0x19
>;
};
..................
};
};
commented out the red colored pad mux and ctrl for uart3_rxd in pinctrl_uart1: uart1grp
In my driver code, i have registered the IRQ handler as below:
irq_num = platform_get_irq(pdev, 0); /* The irq_num for GPIO5_IO26 seems 218 */
if (request_irq(irq_num, my_isr_irq_handler,
IRQF_TRIGGER_RISING, "my_isr", NULL) != 0) {
pr_err("Fail to request my_isr irq interrupt!\n");
return -1;
}
/* My ISR Handler Function */
irqreturn_t my_isr_irq_handler(int irq, void *dev_id)
{
pr_info("%s\n",__func__);
return IRQ_HANDLED;
}
#cat /proc/interrupts
CPU0 CPU1 CPU2 CPU3
218: 0 0 0 0 gpio-mxc 26 Edge my_isr
At J1003, Pin 10, I have applied a pulse of duty 400 usecs. But surprisingly for me the isr handler : my_isr_irq_handler is not invoked.
Could you please help me to resolve this problem.
Thank you, Sreedhar
已解决! 转到解答。
Hi Sreedhar
one can check if interrupt event was registered in gpio interrupt status register described in
sect.8.3.3.7 GPIO interrupt status register (GPIOx_ISR)
i.MX 8M Mini Applications Processor Reference Manual
For debugging one can use memtool
https://source.codeaurora.org/external/imx/imx-test/tree/test/memtool?h=imx_5.4.70_2.3.0
or AN4553 Using Open Source Debugging Tools for Linux on i.MX Processors
Best regards
igor
Hi Sreedhar
one can check if interrupt event was registered in gpio interrupt status register described in
sect.8.3.3.7 GPIO interrupt status register (GPIOx_ISR)
i.MX 8M Mini Applications Processor Reference Manual
For debugging one can use memtool
https://source.codeaurora.org/external/imx/imx-test/tree/test/memtool?h=imx_5.4.70_2.3.0
or AN4553 Using Open Source Debugging Tools for Linux on i.MX Processors
Best regards
igor