Frescale imx U-Boot repositories

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Frescale imx U-Boot repositories

7,784件の閲覧回数
feae
Contributor I

Hello all,

I'd like to know what's the difference between the Frescale imx board
repositories from:

1) https://source.codeaurora.org/external/imx/uboot-imx
2) https://github.com/Freescale/u-boot-fslc

3) http://git.freescale.com/git/cgit.cgi/imx/uboot-imx.git

It seems that #2 is rebased more often and might be supported by the yocto community. I
was wordering if the differece could be in stability or board support.

#1 and #3 seems to be clones

Thanks for your help,
Fernando

0 件の賞賛
返信
1 返信

5,751件の閲覧回数
Carlos_Musich
NXP Employee
NXP Employee

Hi Fernando,

there are BSPs for i.MX processors developed by NXP and there are also BSPs created by a community external to NXP.

You can find the NXP BSPs releases here: git.freescale.com  > fsl-arm-yocto-bsp.git

On the other hand the BSPs releases developed by the external community can be found here: https://github.com/Freescale/

NXP provides support of the BSPs developed by NXP, but unfortunately the releases of the external community are out of our scope.

If you need support on any of the community's releases you may subscribe the FSL Community BSP mailing list at freescale.github.io to talk directly with the developers and other users. Direct link is:
https://lists.yoctoproject.org/listinfo/meta-freescale


Regards,
Carlos
NXP Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信