Frescale imx U-Boot repositories

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Frescale imx U-Boot repositories

7,844 Views
feae
Contributor I

Hello all,

I'd like to know what's the difference between the Frescale imx board
repositories from:

1) https://source.codeaurora.org/external/imx/uboot-imx
2) https://github.com/Freescale/u-boot-fslc

3) http://git.freescale.com/git/cgit.cgi/imx/uboot-imx.git

It seems that #2 is rebased more often and might be supported by the yocto community. I
was wordering if the differece could be in stability or board support.

#1 and #3 seems to be clones

Thanks for your help,
Fernando

0 Kudos
Reply
1 Reply

5,811 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi Fernando,

there are BSPs for i.MX processors developed by NXP and there are also BSPs created by a community external to NXP.

You can find the NXP BSPs releases here: git.freescale.com  > fsl-arm-yocto-bsp.git

On the other hand the BSPs releases developed by the external community can be found here: https://github.com/Freescale/

NXP provides support of the BSPs developed by NXP, but unfortunately the releases of the external community are out of our scope.

If you need support on any of the community's releases you may subscribe the FSL Community BSP mailing list at freescale.github.io to talk directly with the developers and other users. Direct link is:
https://lists.yoctoproject.org/listinfo/meta-freescale


Regards,
Carlos
NXP Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply