Freescale DDR3 script not have the option for to set DDR3-1866 memory type

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Freescale DDR3 script not have the option for to set DDR3-1866 memory type

Jump to solution
1,122 Views
aravinthkumarja
Senior Contributor II

Hi all,

We are using micron DRAM (MT41K256M16) -DDR3-1866 memory type.

For this i need to configure in uboot .cfg file. So i use the below named excel file.

Mx6DQSDL DDR3 Script Aid V0.08.xlsx

But this excel script not have the option of DDR3-1866. So how can i configure this??

Any other updated script is there??

Recommend if anything other script available??

if any other procedure is there guide me??

Regards,

Aravinth

0 Kudos
1 Solution
567 Views
Yuri
NXP Employee
NXP Employee

Hello,

  i.MX6 supports DDR3/LVDDR3/LPDDR2-1066; maximum DRAM frequency

is 533 MHz. Therefore the "more speedy" DRAM parts, should be configured for

533 MHz (1066).

Have a great day,

Yuri

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct

Answer button. Thank you!

------------------------------------------------------------------------------

View solution in original post

0 Kudos
1 Reply
568 Views
Yuri
NXP Employee
NXP Employee

Hello,

  i.MX6 supports DDR3/LVDDR3/LPDDR2-1066; maximum DRAM frequency

is 533 MHz. Therefore the "more speedy" DRAM parts, should be configured for

533 MHz (1066).

Have a great day,

Yuri

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct

Answer button. Thank you!

------------------------------------------------------------------------------

0 Kudos