Hi all,
We are using micron DRAM (MT41K256M16) -DDR3-1866 memory type.
For this i need to configure in uboot .cfg file. So i use the below named excel file.
Mx6DQSDL DDR3 Script Aid V0.08.xlsx
But this excel script not have the option of DDR3-1866. So how can i configure this??
Any other updated script is there??
Recommend if anything other script available??
if any other procedure is there guide me??
Regards,
Aravinth
已解决! 转到解答。
Hello,
i.MX6 supports DDR3/LVDDR3/LPDDR2-1066; maximum DRAM frequency
is 533 MHz. Therefore the "more speedy" DRAM parts, should be configured for
533 MHz (1066).
Have a great day,
Yuri
------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct
Answer button. Thank you!
------------------------------------------------------------------------------
Hello,
i.MX6 supports DDR3/LVDDR3/LPDDR2-1066; maximum DRAM frequency
is 533 MHz. Therefore the "more speedy" DRAM parts, should be configured for
533 MHz (1066).
Have a great day,
Yuri
------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct
Answer button. Thank you!
------------------------------------------------------------------------------