For increasing the capacity of RTC backup battery

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

For increasing the capacity of RTC backup battery

跳至解决方案
1,239 次查看
george
Senior Contributor II

Dear all,

We use i.MX6 for industrial equipment.

The equipment needs RTC.

It has usually stopped for a long time in many cases.

Therefore, in order to keep RTC operation for a long time, it must have a large capacity backup battery.

We use MMPF0100 with i.MX6.

However, the current which can be supplied from MMPF0100 for LICELL charge is 60uA.

Therefore, the charge for the large capacity LICELL cannot be finished within the equipment operation period.

We will change the i.MX6-SDP schematics to which it refers, in order to remove 60uA limitation.

It gets the charging current from GEN_3V3.

Is our schematics available as the file attached here?

Is there any point which takes care?

Best Regards,

George

标签 (1)
0 项奖励
回复
1 解答
961 次查看
igorpadykov
NXP Employee
NXP Employee

Hi George

I looked at attached here picture

and think that such solution is quite feasible.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
962 次查看
igorpadykov
NXP Employee
NXP Employee

Hi George

I looked at attached here picture

and think that such solution is quite feasible.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
961 次查看
george
Senior Contributor II

Dear Igor,

THX

BR,

George

0 项奖励
回复