For fall time of the CORE power1.375V

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

For fall time of the CORE power1.375V

Jump to solution
798 Views
takashitakahash
Contributor III

For fall time of the CORE power1.375V Room temperature,
there is a difference in the fall time
(current consumption) at low temperature. Waveform see attach supplementary materials.

There can be problematic in that cut fell 1.375 V power upon the return from the interruption to 3.1 V power
would stand up
?
(After all of the power is turned on,POR_B will be canceled.)

Must be within 200 ms stood down as the specifications of the product,

but low temperatures at 200 ms after the voltage value is 0.75 V.

Labels (2)
0 Kudos
1 Solution
737 Views
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

discharge time depends on silicon leakage current, which greatly

depends on temperature. Unfortunately this value is not specified.

As workaround one can add external resistor, so there will be guaranteed discharging

current or design some another external discharging circuit.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
1 Reply
738 Views
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

discharge time depends on silicon leakage current, which greatly

depends on temperature. Unfortunately this value is not specified.

As workaround one can add external resistor, so there will be guaranteed discharging

current or design some another external discharging circuit.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos