Yuuki-san !
The packages are not the same. Please refer to corresponding
pages, tab “Package / Quality” for more details about packages.
i.MX6Q|i.MX 6Quad Processors|Quad Core|NXP
http://cache.freescale.com/files/shared/doc/package_info/98ASA00330D.pdf
http://cache.freescale.com/files/shared/doc/package_info/98ASA00329D.pdf
i.MX6DL|i.MX 6DualLite Processors|3D Graphics|NXP
http://cache.freescale.com/files/shared/doc/package_info/98ASA00404D.pdf
Regards,
Yuri.
Yuuki, hello !
" [...] both of them are right, they are different chips, so the package's accuracy have difference,
by the way, the typical value is 0.5mm for both of them, customers just need to set their package
follow this value, I think this have no influence for customers to set the package."
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Dear Yuri-san,
Thank you for your response.
The Ball width for i.MX6DL is Min:φ0.44/Typ:φ0.5/Max:φ0.65.
=>
It seems that tolerance on the Max side is very big.
I suspect that it is Max:φ0.55 not φ0.65.
Would you check it once again?
Best Regards,
Yuuki
Yuuki-san !
The packages are not the same. Please refer to corresponding
pages, tab “Package / Quality” for more details about packages.
i.MX6Q|i.MX 6Quad Processors|Quad Core|NXP
http://cache.freescale.com/files/shared/doc/package_info/98ASA00330D.pdf
http://cache.freescale.com/files/shared/doc/package_info/98ASA00329D.pdf
i.MX6DL|i.MX 6DualLite Processors|3D Graphics|NXP
http://cache.freescale.com/files/shared/doc/package_info/98ASA00404D.pdf
Regards,
Yuri.
Hello,
I forwarded request to the team to double check it.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Just for me :