For Ball Width tolerance for i.MX6 Dual Lite

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

For Ball Width tolerance for i.MX6 Dual Lite

Jump to solution
1,156 Views
yuuki
Senior Contributor II

Daer all,

We design PCB Pad for i.MX6DL.

According to the data sheet for i.MX6DL, Ball width is Min:φ0.44/Typ:φ0.5/Max:φ0.65.

However, in the data sheet for i.MX6Q,  Ball width is φ0.5+/-0.05.

Is the Ball width tolerance for i.MX6DL rigth?

Best Regards,

Yuuki

Labels (1)
0 Kudos
Reply
1 Solution
4 Replies
1,049 Views
Yuri
NXP Employee
NXP Employee

Yuuki, hello !

" [...] both of them are right, they are different chips, so the package's accuracy have difference,
by the way, the typical value is 0.5mm for both of them, customers just need to set their package
follow this value, I think this have no influence for customers to set the package."


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,049 Views
yuuki
Senior Contributor II

Dear Yuri-san,

Thank you for your response.

The Ball width for i.MX6DL is Min:φ0.44/Typ:φ0.5/Max:φ0.65.

=>

It seems that tolerance on the Max side is very big.

I suspect that it is Max:φ0.55 not φ0.65.

Would you check it once again?

Best Regards,

Yuuki

0 Kudos
Reply
1,050 Views
Yuri
NXP Employee
NXP Employee
0 Kudos
Reply
1,049 Views
Yuri
NXP Employee
NXP Employee

Hello,

  I forwarded request to the team to double check it.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

Just for me :

For Ball width tolerance for i.MX6 Dual Lite

0 Kudos
Reply