Hello Community,
I have generated the Custom SCFW for Custom Board based on i.MX8QXP with reference to i.MX8 MEK Board, We are using LPDDR4 and eMMC from different vendor.
PMIC Used: MC33PF8100FJES
I am flashing the SCFW firmware on eMMC using UUU tool using following command:
$ sudo ./uuu -V -b emmc flash.bin
Logs for the above command attached(file name: "uuu_log_with-V.doc")
ISSUE: While flashing the eMMC Card, the USB Port continuously connects and disconnects (Note: All the cables are new, connections are good, the issue happens only when we run UUU command.) dmesg snapshot attached. ( File Name: "dmesg_while_uuu_is_executing.png")
The output of "lsusb" command to which board is connected"
Bus 002 Device 001: ID 1d6b:0003 Linux Foundation 3.0 root hub
Bus 001 Device 005: ID 413c:301a Dell Computer Corp.
Bus 001 Device 004: ID 413c:2113 Dell Computer Corp.
Bus 001 Device 042: ID 0403:6010 Future Technology Devices International, Ltd FT2232C Dual USB-UART/FIFO IC
Bus 001 Device 057: ID 1fc9:012f NXP Semiconductors
Bus 001 Device 006: ID 0cf3:e007 Atheros Communications, Inc.
Bus 001 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub
I have followed the below links to generate the SCFW Firmware:
1. https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8-Boot-process-and-creating-a-bootab...
2. https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/System-Controller-Firmware-101-Getting-s...
Queries:
1. How can I flash the SCFW firmware to eMMC generated using imx-mkimage tool?
2. Why the USB Continuously reboots? Any known issue?
Regards,
Kailas K.
已解决! 转到解答。
Hi Kailas
1. this may be version compatibility issues, please try to rebuild image
from scratch using SCFW version matching linux and other (as described in Release Notes
of each software package on that web link)
2, for usb issues please try to reproduce issue on MEK reference board, to narrow down
problem, this may be due to hardware and one can recheck it with recommendations provided in
i.MX 8QuadMax/i.MX 8QuadXPlus Hardware Developer’s Guide
Best regards
igor
Hello Igor,
I was able to resolve this above issue, Successfully ported the bootable image on Custom Board.
We were using i.MXQXP C0 revision. Issue was resolved by doing the following changes.
Thanks @igorpadykov for your support.
Success Logs:
kailas@kailas:~/mfgtools/uuu$ sudo ./uuu -b emmc /home/kailas/issI_uboot_scfw/imx-mkimage/iMX8QX/flash.bin
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.3.191-0-g4fe24b9
Success 1 Failure 0
3:1 7/ 7 [Done ] FB: Done
Hello Igor,
I am flashing the SCFW image in eMMC using the below command.
$ sudo ./uuu -V -b emmc flash.bin
I have flashed the Uboot using the above command in EVK, But is it the right way to flash SCFW firmware using the above command?
As per the User Guide, SCFW firmware shall be flashed on SD card there is no procedure for eMMC, but for the custom board which we have developed using i.MX8QXP does not have SD card Slot we only have eMMC and Flex Interface for memories.
Can you please provide me with the Flashing procedure for SCFW using eMMC?
Thanks & Regards,
Kailas K.
Hi Kailas
sect.4.3.4 Copying a bootloader image i.MX Linux User’s Guide
is also valid for emmc. Also there are sample uuu scripts in Demo Images
which work with emmc
i.MX 8QuadXPlus(C0) MEK , i.MX 8QuadXPlus(B0) MEK
Also SCFW image is not "flash.bin". flash.bin is full image and SCFW is part of that image
as shown on below link
Best regards
igor
Hi Kailas
>Where I can get the SCFW Binary and SECO FW binary for release 5.4.24_2.1.0?
they are all included in image when one follows guidelines for image building
as shown on below link
Best regards
igor
Hi Kailas
1. this may be version compatibility issues, please try to rebuild image
from scratch using SCFW version matching linux and other (as described in Release Notes
of each software package on that web link)
2, for usb issues please try to reproduce issue on MEK reference board, to narrow down
problem, this may be due to hardware and one can recheck it with recommendations provided in
i.MX 8QuadMax/i.MX 8QuadXPlus Hardware Developer’s Guide
Best regards
igor