Failed to boot i.mx6ul from usdhc2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Failed to boot i.mx6ul from usdhc2

1,071件の閲覧回数
dhvanil_patel1
Senior Contributor I

Hi,

We are developing produce based on i.MX6UL. We are facing an issue while booting the board from uSDHC2 port. We are using below mention pinmux for uSCHD2. We have set the boot config register to boot device from uSDHC2 port along with boot mode setting to internal boot. When we power up the device, The i.MX6UL Boot ROM is not generate any clock on usdhc2.CLK (LCD_DATA19) pin to boot from uSDHC2

#

Name

Default

ALT0ALT8
A13LCD_DATA18gpio3.IO[23]lcdif.DATA[18]usdhc2.CMD
D14LCD_DATA19gpio3.IO[24]lcdif.DATA[19]usdhc2.CLK
C14LCD_DATA20

gpio3.IO[25]

lcdif.DATA[20]usdhc2.DATA0
B14LCD_DATA21gpio3.IO[26]lcdif.DATA[21]usdhc2.DATA1
A14LCD_DATA22gpio3.IO[27]lcdif.DATA[22]usdhc2.DATA2
B16LCD_DATA23gpio3.IO[28]lcdif.DATA[23]usdhc2.DATA3

During debugging, we found,The i.MX6UL boot ROM generates clock on "NAND_RE_B" pin.

Is there any way available to  set Boot ROM to generate CLK on "usdhc2.CLK (LCD_DATA19)"  and boot from uSDHC2 port with above mentioned pin settings?

-

Dhvanil Patel

ラベル(1)
タグ(4)
0 件の賞賛
返信
2 返答(返信)

833件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

one can first boot from spi-nor or other media, then from uSDHC2 port.

Similar approach is given in attached AN4691.

~igor

0 件の賞賛
返信

833件の閲覧回数
durmus
Contributor IV

Hi,

From reference manual section 8.5.3.4 IOMUX Configuration for SD/MMC;

usdhc_boot.jpg

It seems that for USDHC boot you can only use specific pads and not other alternatives.

For your case, booting from USDHC2 seems to be only supported through NAND_... pads.

0 件の賞賛
返信