Fail to read Altera FPGA by i.MX6 through PCIe

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Fail to read Altera FPGA by i.MX6 through PCIe

1,094件の閲覧回数
massohy
Contributor II

Hello,

 

I tried to build loopback system with i.MX6 as RC and Altera FPGA as EP.

I write data from software on Linux, then FPGA will back same data to software .

 

I made test program using user space I/O before making kernel driver at first.

This program was able to write data to FPGA. But I got following error at read data from FPGA.

 

------

Unhandled fault: external abort on non-linefetch (0x1018) at

Bus error

------

 

I am using yocto its kernel version 3.14.52-1.1.1_ga+gdb1bcba.

I set 0x01100000-0x011FFFFFF as BAR0 at FPGA.

 

 

result of lspci

01:00.0 Multimedia video controller: Altera Corporation Device 1001 (rev 01)

                   Subsystem: Altera Corporation Device 1001

                   Flags: bus master, fast devsel, latency 0, IRQ 400

                   Memory at 01100000 (32-bit, non-prefetchable) [size=1M]

                   Capabilities: [50] MSI: Enable+ Count=16/16 Maskable- 64bit+

                   Capabilities: [78] Power Management version 3

                   Capabilities: [80] Express Endpoint, MSI 00

                   Capabilities: [100] Virtual Channel

                   Capabilities: [200] Vendor Specific Information: ID=1172 Rev=0 Len=044 <?>

 

result of cat resource

~# cat /sys/bus/pci/devices/0000\:01\:00.0/resource

0x0000000001100000 0x00000000011fffff 0x0000000000040200

0x0000000000000000 0x0000000000000000 0x0000000000000000

0x0000000000000000 0x0000000000000000 0x0000000000000000

0x0000000000000000 0x0000000000000000 0x0000000000000000

0x0000000000000000 0x0000000000000000 0x0000000000000000

0x0000000000000000 0x0000000000000000 0x0000000000000000

0x0000000000000000 0x0000000000000000 0x0000000000000000

 

A part of my source codes are following,

 

/*######

 

    int barfd;

    void *addrbar0;

 

    barfd = open("/sys/class/uio/uio0/device/resource0", O_RDWR);

    addrbar0 = mmap(NULL, size, PROT_READ|PROT_WRITE, MAP_SHARED, barfd, 0);

    close(barfd);

/* Write to FPGA */

*(unsigned int*)(addrbar0 + cnt) = src_data[cnt];

 

    /* Read from FPGA */

dst_data[cnt] = *(unsigned int*)(addrbar0 + cnt);

 

######*/

 

open function and mmap function was no error occurred.

When I perform writing to FPGA, then it succeeded. But when I perform reading from FPGA, then I got “Bus Error“.

 

What should I do?

 

 

Best Regards,

タグ(1)
0 件の賞賛
2 返答(返信)

735件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 Is it possible to check if data, written to the FPGA, really were accepted? 


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

735件の閲覧回数
massohy
Contributor II

Hello,

Thank you for your reply.

I checked FPGA about write back. I found that FPGA write back address was invalid.

And when I read PCI BAR0 address, then CPU make unnecessary read command to PCIe. Error might be occurred because FPGA was not acceptable.

Best Regards,