Hello
I am using customized board based on NXP IMX6UL EVK board. There is a difference in the part numbers of SOC
----------------------------------------------------------------------
NXP IMX6UL EVK Board
Processor -- MCIMX6G2CVM05AA
---------------------------------------------------------------------
Customized IMX6UL Board
Processor --- MCIMX6G3CVM05AB
--------------------------------------------------------------------
The part numbers of USB, UART , RAM and eMMC are same The part number of RAM is
MT41K256M16TW-107 XIT:P and eMMC is MTFC8GAKAJCN-4M IT TR(8GB Micron). Used the same lines which are used in NXP EVK for eMMC , USB and RAM. I successfully flashed the NXP EVK Board using the UUU tool through USB. The same thing i replicated on my custom board. I am facing the following issue when i am trying to flash the custom board through USB using UUU tool.
ERROR: HID(W) : LIBUSB_ERROR_TIMEOUT
Are there any differences in between MCIMX6G2CVM05AA and MCIMX6G3CVM05AB SOC's ? Do we have to make any modifications based on the difference of part numbers in SOC's ?
Please let me know if any
Thanks & Regards
Shamiullah