hello,
recently,I also do some work about FT5X06,my IC is FT5506 ,the kernel of my Android system is linux-3.0.35 ,but the screen can't work ,there is no reflect when I touch the screen ,then I checked it ,it seem that the interrupt of touch ic has problem .the some files or message as follows:
can you give me some advice about this? Thank you !
Hi peng
please look at FT5X06 and touchscreen links
https://community.freescale.com/thread/293210
https://community.nxp.com/message/624165
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
hello,I want to kown whether the SD1_CMD/GPIO1_IO18 pin can use as the interrupt pin.