Dear all,
is there any way available to fasten the flashing method through ATK tool. My problem would be that To load the (uboot.bin,uImage,rootfs) through serial its taking so many time to complete to NAND.
is there any way to flash the code through Ethernet interface ? or any tool is available to flashing in less time and multiple device at the same time ?
How can i flash the software to multiple boards in less time. please give me suggestion and solutions.
Regards,
Guru
The ATK can load data via USB (OTG) port. Multiple targets - alas - are not supported.
For recent i.MX devices the MFG is recommended.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Dear Yuri,
I am using i.MX25 3 stack board for my development. So Now I am flashing through debug board to core board via serial.
Debug board having only uart,ethernel option there is no OTG interface.
How can I use OTG for i.MX25 board for ATK tool?
Regards,
Guru
Personal board of the i.MX25 PDK has OTG connector. Please use it.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Dear Yuri,
I tried that way only I connected the usb cable also from PC to board OTG connection. but in ATK tool saying that No usb detected. Please check with USB connection.
Please give me an idea . what was the mistake?
How can I proceed to do that ?
Regards,
Guru
Looks like You need to install USB driver for the ATK. Please follow section
"Installation and uninstall of USB Drivers" in ATK documentation.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Dear Yuri,
will ATK tool support win7, 64bit for USB ?
Is any another way is available to flash the sw files such as uboot.bin,uImage,rfs through Ethernet interface to NAND,SDCARD.
This way is very useful to be done the work very faster.
Regards,
Guru
Please take a look at the following regarding the ATK.
The ATK Toolkit is not supported anymore.
The customer will have to switch to the Manufacturing Tool called MFG.
MFG Tool will be the main tool to flash / run images on a board.
MFG Tool is available now in a version that supports Win7 in 64bit.
In the recent MFG release there are 2 .exe files: mfgtool and mfgtool2.
mfgtool is intended for I.MX25,27,28,31,35, 50,53.
mfgtool2 is for i.mx6 seriels
mfgtool.exe can work at USB3.0 and 2.0
For example the following link contains i.MX25 MFG.
MX25 3stack HAB (High Assurance Boot)
As for Ethernet - it is usual way to load U-boot via UART and use U-boot Ethernet options for further operations.
Sorry, direct OS deployment via Ethernet is not supported under i.MX bootloaders.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Dear Yuri,
Thanks for explained clearly.
I have downloaded the mfg tool for the below link
http://www.freescale.com/webapp/sps/site/overview.jsp?code=IMX_DESIGN
I tried use it but This tool doesn't support the imx25 option on the ui . what should I need to do for I.MX25 to use mfg tool
Please give me an idea to implement this.
Regards,
Guru