External watchdog for imx6 u-boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

External watchdog for imx6 u-boot

1,145 Views
konstantyn75
Contributor II

Hello,

I'm using external watchdog MAX6751 for imx6q board and i need to trigger it in u-boot, otherwise system would reset. The reset time is about 1 sec.

I've added initialization of GPIO PAD to the board support code and function hw_watchdog_reset(). When i enable CONFIG_HW_WATCHDOG and compile u-boot, it does not load at all. When i disable CONFIG_HW_WATCHSOG, everything boots fine.

Did anybody have any issues of auto-triggering watchdogs in u-boot?

Thanks a lot

Konstantyn

Labels (3)
0 Kudos
2 Replies

992 Views
konstantyn75
Contributor II

Hi Igor, thank you very much. I'll ask this question on u-boot forum. I was just hoping somebody from NXP community had the same problem and it is imx6 related.

Regards,

Konstantyn

0 Kudos

992 Views
igorpadykov
NXP Employee
NXP Employee

Hi Konstantyn

nxp uboot does not use external wdog and since this is not imx specific

question it may be posted on uboot mail list

U-Boot Info Page 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos