External dimensions of MCIMX7SABRE

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

External dimensions of MCIMX7SABRE

跳至解决方案
1,008 次查看
ko-hey
Senior Contributor II

Hi all

Does someone have a information for external dimensions of MCIMX7SABRE ?

Ko-hey

标签 (3)
1 解答
855 次查看
jan_spurek
NXP Employee
NXP Employee

Hello Ko-hey,

the dimensions are ca 130x130 mm.

Best Regards,

Jan

在原帖中查看解决方案

4 回复数
856 次查看
jan_spurek
NXP Employee
NXP Employee

Hello Ko-hey,

the dimensions are ca 130x130 mm.

Best Regards,

Jan

855 次查看
ko-hey
Senior Contributor II

Hi janspurek

Thank you for support.

Could you tell me the following things too ?

1.Position of 120 pin connector J13 (QSH - 060 - 01 - L - D - A)
2.Position and hole diameter of non-through hole at four corners
3.Substrate thickness

Ko-hey

0 项奖励
回复
855 次查看
jan_spurek
NXP Employee
NXP Employee

Hello Ko-hey,

1.    -151.771, 3746.522 [mills]

2.    diameter: ca 127 mills

       hole 1: -236.220, 4960.630 [mills]

       hole 2: 4566.929, 4960.630 [mills]

       hole 3: 4566.929, 157.480 [mills]

       hole 4: -236.220, 157.480 [mills]

3.    56 mills (dielectrics only - each 8 mills), 65.6 mills (including the conductor layers - each 1.2 mills)

Please note that the coordinates apply to the centers of the objects.

Best Regards,

Jan

855 次查看
ko-hey
Senior Contributor II

Hi janspurek

Thank you for the useful info!!

Ko-hey

0 项奖励
回复