Execute NEON instructions on i.MX6 SABRE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Execute NEON instructions on i.MX6 SABRE

699件の閲覧回数
prem_chandh
Contributor I

Hi,
       I'm using Freescale(Now NXP) MCIMX6Q-SDB Evalution Board.I'm trying to bring up the board.So initially trying some sample programs.I Can able to execute and Print the sample Helloworld Program in Console. In next step I'm trying to execute some NEON Instructions. I followed the Procedure given in Tutorials( link) to execute. But i can't able to get the result.But my code is building and generating .axf file with NEON instructions. Please help me for the same.

I'm using DS-5 Development Studio as IDE and D-Stream Debug Hardware.


Thanks

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 返信

574件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 

  I hope some considerations and example of the following thread help.

Integrating Processor Expert for i.MX and ARM GCC with Eclipse 

  Look at "init_MMU.s" regarding NEON initialization.

 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

0 件の賞賛
返信