Ethernet

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Ethernet

625件の閲覧回数
saida
Contributor II

hi i.mx6 community

i have sabresd board duallite

im my custom board i have ethenet phy dp83848 and magnetic is hx1148. and i am configuring transceiver in MII10 mode in u-boot-2015.01 and  also configured related IO MUX PADS

now i set ipaddr, serverip and ethaddr environment variables in u-boot. this mac is from my sabresd board.

now when i do  #ping serverip

i am getting this error

ARP Retry count exceded : starting again

i am able to read mii registers and the same procedure as i mentioned above is working for sabresd board

so what could be the error, or if i am doing any mistake please help me in this regard or is there any hardware problem ? (my chassis ground is in floating)

please any one can help in this regard so that my custom board will the OK with all my required peripherals

thank you

SAIDA

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

487件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Saida S,

I would recommend reviewing the software configuration. Since you are using a different PHY than the SABRE board you would need to change the U-Boot configuration and Driver in order to accommodate the new PHY. There is some information on the driver configuration on the manufacturer’s website.

Regards,

0 件の賞賛
返信

487件の閲覧回数
saida
Contributor II

hi

thank you

i sorted out the problem

regards

saida

0 件の賞賛
返信